<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックRe: CMISI interrupt priority</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/CMISI-interrupt-priority/m-p/1025450#M2162</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tobias,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am very happy that the problem has been resolved. Unfortunately, there are no examples with that specific functionality that show the use of NVIC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you have any questions please don't hesitate to ask.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Jan 2020 20:22:17 GMT</pubDate>
    <dc:creator>nxf58474</dc:creator>
    <dc:date>2020-01-20T20:22:17Z</dc:date>
    <item>
      <title>CMISI interrupt priority</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/CMISI-interrupt-priority/m-p/1025448#M2160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I work on a Kinetis MKE18F512 with SDK 2.6 and&amp;nbsp; now I have problems to understand and use the interrupts in a correct way.&lt;BR /&gt;My Problem:&lt;/P&gt;&lt;P&gt;I have interrupt settings at reset state.&lt;BR /&gt;I drive a system-timer wit the sysTick interrupt. Now if I use a UART transfer the sysTick don't run and I don't get any timings.&lt;BR /&gt;It also don't help to lower the UART interrupt priority by &lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;   &lt;SPAN class="token function"&gt;NVIC_SetPriority&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; LPUART0_TX_IRQn&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
   &lt;SPAN class="token function"&gt;NVIC_SetPriority&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; LPUART0_RX_IRQn&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
   &lt;SPAN class="token function"&gt;NVIC_SetPriority&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; CAN0_ORed_IRQn&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
   &lt;SPAN class="token function"&gt;NVIC_SetPriority&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; CAN0_Error_IRQn&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
   &lt;SPAN class="token function"&gt;NVIC_SetPriority&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; CAN0_Wake_Up_IRQn&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
   &lt;SPAN class="token function"&gt;NVIC_SetPriority&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; CAN0_ORed_Message_buffer_IRQn&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;If one interrupt is running no other will be called.&lt;BR /&gt;How could I setup that the systick interrupt can preempt all others?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2020 09:22:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/CMISI-interrupt-priority/m-p/1025448#M2160</guid>
      <dc:creator>tobias_mrs</dc:creator>
      <dc:date>2020-01-17T09:22:05Z</dc:date>
    </item>
    <item>
      <title>Re: CMISI interrupt priority</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/CMISI-interrupt-priority/m-p/1025449#M2161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have found the problem:&lt;/P&gt;&lt;P&gt;The function SysTick_Config(uint32_t ticks) set the interrupt priority of the sysTick to 15. That means the lowest priority.&lt;/P&gt;&lt;P&gt;The solution was to reset the priority after calling the init function&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;    &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;!=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;SysTick_Config&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; SystemCoreClock &lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1000&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        ret &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; HAL_ERR_INIT&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
    &lt;SPAN class="keyword token"&gt;else&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        &lt;SPAN class="token function"&gt;NVIC_SetPriority&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; SysTick_IRQn&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
        &lt;SPAN class="comment token"&gt;// no errors&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;  &lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;Bu for further information's. &lt;BR /&gt;Could you lead me to a example how to configure the interrupt priority with the SDK.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2020 09:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/CMISI-interrupt-priority/m-p/1025449#M2161</guid>
      <dc:creator>tobias_mrs</dc:creator>
      <dc:date>2020-01-17T09:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: CMISI interrupt priority</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/CMISI-interrupt-priority/m-p/1025450#M2162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tobias,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am very happy that the problem has been resolved. Unfortunately, there are no examples with that specific functionality that show the use of NVIC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you have any questions please don't hesitate to ask.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jan 2020 20:22:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/CMISI-interrupt-priority/m-p/1025450#M2162</guid>
      <dc:creator>nxf58474</dc:creator>
      <dc:date>2020-01-20T20:22:17Z</dc:date>
    </item>
  </channel>
</rss>