<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GPIO driver Port Read in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/GPIO-driver-Port-Read/m-p/1011046#M2077</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there a specific reason to why there is no function for reading multiple GPIO pins at once in the GPIO driver fsl_gpio.c/h? There are functions to set and clear multiple pins at once but no function for reading.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In general I think that Scott Millers &lt;A _jive_internal="true" href="https://community.nxp.com/message/1129160"&gt;post &lt;/A&gt;from almost one year ago (which also mentioned the GPIO read function which is still missing) is still valid. The documentation is missing a lot of information, links don't work and there is no way to see from the open online API to which processor it refers. As a newcomer to the NXP IMXRT family it is difficult to get started with the processor family and the API. I have to switch between API, MCU Reference Manual and source code quite a lot to understand what is going on and what the correct parameters are. Yes, there are a lot of working code examples for the peripherals which you can create with MCUXpresso Config Tools but they don't show everything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Stefan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jan 2020 13:22:47 GMT</pubDate>
    <dc:creator>imxrtuser</dc:creator>
    <dc:date>2020-01-28T13:22:47Z</dc:date>
    <item>
      <title>GPIO driver Port Read</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/GPIO-driver-Port-Read/m-p/1011046#M2077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is there a specific reason to why there is no function for reading multiple GPIO pins at once in the GPIO driver fsl_gpio.c/h? There are functions to set and clear multiple pins at once but no function for reading.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In general I think that Scott Millers &lt;A _jive_internal="true" href="https://community.nxp.com/message/1129160"&gt;post &lt;/A&gt;from almost one year ago (which also mentioned the GPIO read function which is still missing) is still valid. The documentation is missing a lot of information, links don't work and there is no way to see from the open online API to which processor it refers. As a newcomer to the NXP IMXRT family it is difficult to get started with the processor family and the API. I have to switch between API, MCU Reference Manual and source code quite a lot to understand what is going on and what the correct parameters are. Yes, there are a lot of working code examples for the peripherals which you can create with MCUXpresso Config Tools but they don't show everything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Stefan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2020 13:22:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/GPIO-driver-Port-Read/m-p/1011046#M2077</guid>
      <dc:creator>imxrtuser</dc:creator>
      <dc:date>2020-01-28T13:22:47Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO driver Port Read</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/GPIO-driver-Port-Read/m-p/1011047#M2078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Stefan,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the i.MXRT the concept of Port doesn't exist, like in Kinetis or LPC. Therefore when you want to read a GPIO you need to read a specific PAD.&amp;nbsp;The GPIO module of the RTs was inherited from the i.MX.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jan 2020 18:04:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/GPIO-driver-Port-Read/m-p/1011047#M2078</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2020-01-31T18:04:57Z</dc:date>
    </item>
  </channel>
</rss>