<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FLEXCAN max baudrate in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXCAN-max-baudrate/m-p/973399#M1870</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi sean bzd&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FlexCan Module (without FD) goes hand in hand with the CAN standard 2.0 which is p&lt;SPAN class=""&gt;rogrammable bit rate up to 1 Mb/sec. The FlexCan module with FD support &lt;SPAN class=""&gt;implements the CAN protocol according to the ISO 11898-1 standard and CAN 2.0 B&lt;/SPAN&gt; which is 8 Mb/sec.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;This max baud rate should be achievable but you need to verify the clock source and the possible dividers and multiplier.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hope this information could help you.&lt;/SPAN&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jul 2019 21:17:04 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2019-07-12T21:17:04Z</dc:date>
    <item>
      <title>FLEXCAN max baudrate</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXCAN-max-baudrate/m-p/973398#M1869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the MIMXRT1064-EVK. Looks like the default baudrate for the CANFD is set to 2 Mbps in the demo example. Can someone tell me:&lt;/P&gt;&lt;P&gt;1)What is the max baudrate supported by this eval kit?&lt;/P&gt;&lt;P&gt;2)Can that max baudrate be achieved simply by setting the&amp;nbsp;flexcanConfig.baudRateFD in the example code? or is there more to it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2019 13:01:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXCAN-max-baudrate/m-p/973398#M1869</guid>
      <dc:creator>seanbzd</dc:creator>
      <dc:date>2019-07-11T13:01:06Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXCAN max baudrate</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXCAN-max-baudrate/m-p/973399#M1870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi sean bzd&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FlexCan Module (without FD) goes hand in hand with the CAN standard 2.0 which is p&lt;SPAN class=""&gt;rogrammable bit rate up to 1 Mb/sec. The FlexCan module with FD support &lt;SPAN class=""&gt;implements the CAN protocol according to the ISO 11898-1 standard and CAN 2.0 B&lt;/SPAN&gt; which is 8 Mb/sec.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;This max baud rate should be achievable but you need to verify the clock source and the possible dividers and multiplier.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hope this information could help you.&lt;/SPAN&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jul 2019 21:17:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXCAN-max-baudrate/m-p/973399#M1870</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-07-12T21:17:04Z</dc:date>
    </item>
  </channel>
</rss>