<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flexbus example fails in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Flexbus-example-fails/m-p/679026#M186</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've downloaded an MCUXpresso 2.2 SDK for the TWR-K64F120M. I imported the flexbus driver example and successfully compiled and loaded the code. When I run the code, it prints out:&amp;nbsp;&lt;/P&gt;&lt;P&gt;FLEXBUS Example.&lt;/P&gt;&lt;P&gt;Initialize FLEXBUS.&lt;/P&gt;&lt;P&gt;Start write/read MRAM.&lt;/P&gt;&lt;P&gt;FLEXBUS (MRAM) test: failed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I haven't modified any code, so I would expect it to succeed. Has anyone else had this work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the flexbus working correctly on the same board using the KDS3.0 and KSDK1.3.0. I was trying to port this working code to the new MCUXpresso environment and was having issues, so I figured I would build the example to use as a reference. Since the example doesn't work, it doesn't serve as a useful reference.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jun 2017 17:51:40 GMT</pubDate>
    <dc:creator>yorknh</dc:creator>
    <dc:date>2017-06-07T17:51:40Z</dc:date>
    <item>
      <title>Flexbus example fails</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Flexbus-example-fails/m-p/679026#M186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've downloaded an MCUXpresso 2.2 SDK for the TWR-K64F120M. I imported the flexbus driver example and successfully compiled and loaded the code. When I run the code, it prints out:&amp;nbsp;&lt;/P&gt;&lt;P&gt;FLEXBUS Example.&lt;/P&gt;&lt;P&gt;Initialize FLEXBUS.&lt;/P&gt;&lt;P&gt;Start write/read MRAM.&lt;/P&gt;&lt;P&gt;FLEXBUS (MRAM) test: failed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I haven't modified any code, so I would expect it to succeed. Has anyone else had this work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the flexbus working correctly on the same board using the KDS3.0 and KSDK1.3.0. I was trying to port this working code to the new MCUXpresso environment and was having issues, so I figured I would build the example to use as a reference. Since the example doesn't work, it doesn't serve as a useful reference.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 17:51:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Flexbus-example-fails/m-p/679026#M186</guid>
      <dc:creator>yorknh</dc:creator>
      <dc:date>2017-06-07T17:51:40Z</dc:date>
    </item>
    <item>
      <title>Re: Flexbus example fails</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Flexbus-example-fails/m-p/679027#M187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Larry:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did a quick check about this demo, it works on my side. I would suggest you check the jumper settings in your TWR-MEM board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/23646i7BF8EC4E2AC23976/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jun 2017 08:34:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Flexbus-example-fails/m-p/679027#M187</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-06-19T08:34:45Z</dc:date>
    </item>
  </channel>
</rss>