<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCU-BOOT middleware missing from New Project in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/MCU-BOOT-middleware-missing-from-New-Project/m-p/952870#M1726</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ivekengineer,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to consult this with our SDK team and will update this thread as soon as I have their feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jul 2019 07:39:40 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2019-07-24T07:39:40Z</dc:date>
    <item>
      <title>MCU-BOOT middleware missing from New Project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/MCU-BOOT-middleware-missing-from-New-Project/m-p/952869#M1725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recently downloaded SDK 2.6.0 for an MKV58 device.&amp;nbsp; When I built the SDK, I chose the mcu-boot middleware component.&amp;nbsp; The component is in the SDK zip file.&amp;nbsp; However, when I attempt to create a New Project using MCUXpresso, MCU-BOOT is not an available middleware component to select.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviously, I can build my own generic project and use the source code to achieve what I want, but I seem to remember this being a managed component option in the past?&amp;nbsp; is this a bug, or is the middleware component only available as source code that I have to manually import?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jul 2019 13:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/MCU-BOOT-middleware-missing-from-New-Project/m-p/952869#M1725</guid>
      <dc:creator>ivekengineer</dc:creator>
      <dc:date>2019-07-22T13:45:00Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-BOOT middleware missing from New Project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/MCU-BOOT-middleware-missing-from-New-Project/m-p/952870#M1726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ivekengineer,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to consult this with our SDK team and will update this thread as soon as I have their feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jul 2019 07:39:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/MCU-BOOT-middleware-missing-from-New-Project/m-p/952870#M1726</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2019-07-24T07:39:40Z</dc:date>
    </item>
  </channel>
</rss>