<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FLEXIO_CAMERA_Init in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXIO-CAMERA-Init/m-p/871702#M1317</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wenda:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The flexio interface is for Kinetis parts. Not sure this example has ported to i.mx RT .&lt;/P&gt;&lt;P&gt;The i.MX RT1050 processor has the special camera sensor interface (CSI) module, especially meant for parallel camera connection. So, there is no need of using FlexIO modules.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the example of the CSI module use, please refer to the AN12110 Application note and the corresponding example, available on below link&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12110.pdf" title="https://www.nxp.com/docs/en/application-note/AN12110.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12110.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/77140iA948F08F10C66627/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jan 2019 06:47:13 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2019-01-15T06:47:13Z</dc:date>
    <item>
      <title>FLEXIO_CAMERA_Init</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXIO-CAMERA-Init/m-p/871699#M1314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;请问这个函数是在哪个文件里？&lt;/P&gt;&lt;P&gt;这个文件那里可以下载到。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which file includes this function?&lt;/P&gt;&lt;P&gt;where can I get this file?&lt;/P&gt;&lt;P&gt;I really need this lib, please, thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 Jan 2019 03:46:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXIO-CAMERA-Init/m-p/871699#M1314</guid>
      <dc:creator>1104883515</dc:creator>
      <dc:date>2019-01-13T03:46:08Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXIO_CAMERA_Init</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXIO-CAMERA-Init/m-p/871700#M1315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;RT1052, can you tell me where I can get these libs(&lt;SPAN&gt;fsl_flexio_camera,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;fsl_flexio_camera_adapter,fsl_flexio_camera_edma&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 02:59:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXIO-CAMERA-Init/m-p/871700#M1315</guid>
      <dc:creator>1104883515</dc:creator>
      <dc:date>2019-01-15T02:59:53Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXIO_CAMERA_Init</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXIO-CAMERA-Init/m-p/871701#M1316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me check this issue and will update you later&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 06:22:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXIO-CAMERA-Init/m-p/871701#M1316</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2019-01-15T06:22:28Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXIO_CAMERA_Init</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXIO-CAMERA-Init/m-p/871702#M1317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wenda:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The flexio interface is for Kinetis parts. Not sure this example has ported to i.mx RT .&lt;/P&gt;&lt;P&gt;The i.MX RT1050 processor has the special camera sensor interface (CSI) module, especially meant for parallel camera connection. So, there is no need of using FlexIO modules.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the example of the CSI module use, please refer to the AN12110 Application note and the corresponding example, available on below link&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12110.pdf" title="https://www.nxp.com/docs/en/application-note/AN12110.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12110.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/77140iA948F08F10C66627/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 06:47:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FLEXIO-CAMERA-Init/m-p/871702#M1317</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2019-01-15T06:47:13Z</dc:date>
    </item>
  </channel>
</rss>