<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I2C DMA driver problem in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/I2C-DMA-driver-problem/m-p/851849#M1180</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made a FreeRTOS I2C DMA implementation (based on the SDK i2c DMA driver example) and it is running fine. But...&lt;/P&gt;&lt;P&gt;...But I found a problem that I think is worth being reviewed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While sending data (in my case:&amp;nbsp;&amp;nbsp;start + 1 slave address byte+&amp;nbsp;1subaddress byte&amp;nbsp; + 1 data byte), "I2C_RunDMATransfer" function is called more than one time and almost simultaneously&amp;nbsp; "I2C_RunTransferStateMachineDMA" is also called by the IRQ ("I2C_MasterTransferDMAHandleIRQ"). It happens that both functions can change the "remainingBytesDMA" variable. So, when&amp;nbsp;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;I2C_RunDMATransfer" is called, the "&lt;SPAN&gt;remainingBytesDMA" is 1 and before &lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;I2C_RunDMATransfer" ends the&amp;nbsp;"remainingBytesDMA" variable is changed to 0, then in the end of&amp;nbsp;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;I2C_RunDMATransfer" that operation "handle-&amp;gt;remainingBytesDMA -= transfer_size;" is made and the&amp;nbsp;&lt;SPAN&gt;"remainingBytesDMA" goes from 0 to a very big number and later "DMA_PrepareTransfer" asserts in "(xfer_count &amp;lt;= DMA_MAX_TRANSFER_COUNT) &amp;amp;&amp;amp; (0 == transferBytes % byteWidth)"&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;As a workaround&amp;nbsp;I made the following change in "I2C_RunDMATransfer":&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;changed this
&lt;SPAN class="token function"&gt;DMA_SubmitTransfer&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;dmaHandle&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;xferConfig&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;DMA_StartTransfer&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;dmaHandle&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;remainingBytesDMA &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; transfer_size&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;buf &lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; transfer_size&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;    


to that
&lt;SPAN class="token function"&gt;DMA_SubmitTransfer&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;dmaHandle&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;xferConfig&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;DMA_StartTransfer&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;dmaHandle&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;remainingBytesDMA &lt;SPAN class="operator token"&gt;&amp;gt;=&lt;/SPAN&gt; transfer_size&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;remainingBytesDMA &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; transfer_size&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;else&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;remainingBytesDMA &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;buf &lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; transfer_size&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;In the attached file I have the FreeRTOS inplementation, if you need it.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Apr 2019 08:35:52 GMT</pubDate>
    <dc:creator>microcris</dc:creator>
    <dc:date>2019-04-09T08:35:52Z</dc:date>
    <item>
      <title>I2C DMA driver problem</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/I2C-DMA-driver-problem/m-p/851849#M1180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made a FreeRTOS I2C DMA implementation (based on the SDK i2c DMA driver example) and it is running fine. But...&lt;/P&gt;&lt;P&gt;...But I found a problem that I think is worth being reviewed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While sending data (in my case:&amp;nbsp;&amp;nbsp;start + 1 slave address byte+&amp;nbsp;1subaddress byte&amp;nbsp; + 1 data byte), "I2C_RunDMATransfer" function is called more than one time and almost simultaneously&amp;nbsp; "I2C_RunTransferStateMachineDMA" is also called by the IRQ ("I2C_MasterTransferDMAHandleIRQ"). It happens that both functions can change the "remainingBytesDMA" variable. So, when&amp;nbsp;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;I2C_RunDMATransfer" is called, the "&lt;SPAN&gt;remainingBytesDMA" is 1 and before &lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;I2C_RunDMATransfer" ends the&amp;nbsp;"remainingBytesDMA" variable is changed to 0, then in the end of&amp;nbsp;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;SPAN&gt;I2C_RunDMATransfer" that operation "handle-&amp;gt;remainingBytesDMA -= transfer_size;" is made and the&amp;nbsp;&lt;SPAN&gt;"remainingBytesDMA" goes from 0 to a very big number and later "DMA_PrepareTransfer" asserts in "(xfer_count &amp;lt;= DMA_MAX_TRANSFER_COUNT) &amp;amp;&amp;amp; (0 == transferBytes % byteWidth)"&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;As a workaround&amp;nbsp;I made the following change in "I2C_RunDMATransfer":&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;changed this
&lt;SPAN class="token function"&gt;DMA_SubmitTransfer&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;dmaHandle&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;xferConfig&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;DMA_StartTransfer&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;dmaHandle&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;remainingBytesDMA &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; transfer_size&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;buf &lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; transfer_size&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;    


to that
&lt;SPAN class="token function"&gt;DMA_SubmitTransfer&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;dmaHandle&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;xferConfig&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;DMA_StartTransfer&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;dmaHandle&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;remainingBytesDMA &lt;SPAN class="operator token"&gt;&amp;gt;=&lt;/SPAN&gt; transfer_size&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;remainingBytesDMA &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; transfer_size&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;else&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;remainingBytesDMA &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
handle&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;buf &lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; transfer_size&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;In the attached file I have the FreeRTOS inplementation, if you need it.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2019 08:35:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/I2C-DMA-driver-problem/m-p/851849#M1180</guid>
      <dc:creator>microcris</dc:creator>
      <dc:date>2019-04-09T08:35:52Z</dc:date>
    </item>
    <item>
      <title>Re: I2C DMA driver problem</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/I2C-DMA-driver-problem/m-p/851850#M1181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&amp;nbsp; &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="336982" data-username="microcris" href="https://community.nxp.com/people/microcris"&gt;Cristiano:&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your feedback, could you please let me know the MCU you used and the SDK version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 05:28:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/I2C-DMA-driver-problem/m-p/851850#M1181</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2019-04-24T05:28:46Z</dc:date>
    </item>
    <item>
      <title>Re: I2C DMA driver problem</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/I2C-DMA-driver-problem/m-p/851851#M1182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here it is:&lt;/P&gt;&lt;P&gt;LPC54628J512&lt;/P&gt;&lt;P&gt;SDK2.5.0&lt;/P&gt;&lt;P&gt;I2C DMA driver version 2.0.3&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 13:38:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/I2C-DMA-driver-problem/m-p/851851#M1182</guid>
      <dc:creator>microcris</dc:creator>
      <dc:date>2019-04-24T13:38:21Z</dc:date>
    </item>
  </channel>
</rss>