<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FatFs update? in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/FatFs-update/m-p/815682#M1014</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; Tom:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest SDK version is 2.5.0.&lt;/P&gt;&lt;P&gt;The fatfs version is R0.13b (April 07, 2018)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you click the 'Refresh SDK'&lt;/P&gt;&lt;P&gt;The will be a SDK component management wizard will guide you through the update process. Like this&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70957i1ED55DC811096E38/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I think you have an option to not updated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Dec 2018 08:27:47 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2018-12-26T08:27:47Z</dc:date>
    <item>
      <title>FatFs update?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FatFs-update/m-p/815681#M1013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the RT1050-EVK and the SDK I created has FatFs, but it is an older version that does not allow f_open (RW), only Read or Write. There are a number of improvements like more conventional syntax for mount points.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know I could just include the newer version of FatFs in my project, but I like the glue that MCUXpresso provides with the devices I enable as needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SDK version is R0.12c and the current release is R0.13c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I swap out the files and I "Refresh SDK" will the files get reverted to the older version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not critical at this point, as development has just started...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Nov 2018 14:49:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FatFs-update/m-p/815681#M1013</guid>
      <dc:creator>w2vy</dc:creator>
      <dc:date>2018-11-29T14:49:18Z</dc:date>
    </item>
    <item>
      <title>Re: FatFs update?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FatFs-update/m-p/815682#M1014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; Tom:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest SDK version is 2.5.0.&lt;/P&gt;&lt;P&gt;The fatfs version is R0.13b (April 07, 2018)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you click the 'Refresh SDK'&lt;/P&gt;&lt;P&gt;The will be a SDK component management wizard will guide you through the update process. Like this&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70957i1ED55DC811096E38/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I think you have an option to not updated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Dec 2018 08:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FatFs-update/m-p/815682#M1014</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2018-12-26T08:27:47Z</dc:date>
    </item>
  </channel>
</rss>