<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: installing MCUExpresso IDE under openSuSE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/installing-MCUExpresso-IDE-under-openSuSE/m-p/1819921#M9556</link>
    <description>&lt;P&gt;Solved!&amp;nbsp; After installing an upgrade to openSuSE Linux Leap 15.5 and doing the 781 updates, I was hoping that an appropriate path or link was re-set, still Nothing.&amp;nbsp; Then I installed the full generic Eclipse C development system.&amp;nbsp; Ran it again, and it did install the files but no menu entry, but that was easy to fix.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 02 Mar 2024 21:02:12 GMT</pubDate>
    <dc:creator>ve3id</dc:creator>
    <dc:date>2024-03-02T21:02:12Z</dc:date>
    <item>
      <title>installing MCUExpresso IDE under openSuSE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/installing-MCUExpresso-IDE-under-openSuSE/m-p/1819598#M9552</link>
      <description>&lt;P&gt;I made the tactical error of upgrading mcuexpressoide from 11.8.1 to 11.9.0&amp;nbsp; in the middle of a project, hoping it would resolve some minor issues.&lt;/P&gt;&lt;P&gt;I know the deb.bin file is for debian-based systems, but it has been installing fine on my openSuSE Leap 15.3 and 15.4 for a year or two now, since ide&amp;nbsp; 11.5 in fact.&lt;/P&gt;&lt;P&gt;So I downloaded the update and installed it, replacing 11.8.1.&amp;nbsp; At first it worked no problem, but after a reboot, it cannot find the binary.&amp;nbsp; Nor can I find it manually.&lt;/P&gt;&lt;P&gt;So I tried installing again (11.9.0 over 11.9.0) and 1) it failed to find libc6, which I expect since it should use glibc, and dozens of dependencies not met. That should only affect jlink, which I do not use.&lt;/P&gt;&lt;P&gt;I can't understand how 11.5 and 11.8 could have loaded fine (and let me get thousands of lines into my project) and not now.&amp;nbsp; I reasoned that there must be a symlink missing, but no idea what or where!&lt;/P&gt;&lt;P&gt;Has anybody else experienced this?&lt;/P&gt;&lt;P&gt;Any help really appreciated.&lt;/P&gt;&lt;P&gt;cheers,&lt;/P&gt;&lt;P&gt;Nigel Johnson&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 13:56:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/installing-MCUExpresso-IDE-under-openSuSE/m-p/1819598#M9552</guid>
      <dc:creator>ve3id</dc:creator>
      <dc:date>2024-03-01T13:56:38Z</dc:date>
    </item>
    <item>
      <title>Re: installing MCUExpresso IDE under openSuSE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/installing-MCUExpresso-IDE-under-openSuSE/m-p/1819599#M9553</link>
      <description>&lt;P&gt;I should add that I went back and tried to re-install 11.8 with the same errors&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 13:58:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/installing-MCUExpresso-IDE-under-openSuSE/m-p/1819599#M9553</guid>
      <dc:creator>ve3id</dc:creator>
      <dc:date>2024-03-01T13:58:01Z</dc:date>
    </item>
    <item>
      <title>Re: installing MCUExpresso IDE under openSuSE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/installing-MCUExpresso-IDE-under-openSuSE/m-p/1819921#M9556</link>
      <description>&lt;P&gt;Solved!&amp;nbsp; After installing an upgrade to openSuSE Linux Leap 15.5 and doing the 781 updates, I was hoping that an appropriate path or link was re-set, still Nothing.&amp;nbsp; Then I installed the full generic Eclipse C development system.&amp;nbsp; Ran it again, and it did install the files but no menu entry, but that was easy to fix.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 02 Mar 2024 21:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/installing-MCUExpresso-IDE-under-openSuSE/m-p/1819921#M9556</guid>
      <dc:creator>ve3id</dc:creator>
      <dc:date>2024-03-02T21:02:12Z</dc:date>
    </item>
  </channel>
</rss>