<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: XIP folder files undesired update using Configuration Tool</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1798409#M9489</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;thank you for your answer.&lt;/P&gt;&lt;P&gt;I have regenerated the MEX file for my project but - again - every time I add a new component from SDK all the files are updated:&lt;/P&gt;&lt;P&gt;- XIP folder files.&lt;/P&gt;&lt;P&gt;- startup.c (I relocate flexRAM, so I added modifications to startup_mimxrt1052.c)&lt;/P&gt;&lt;P&gt;- board.c (I relocate flexRAM, so I have to reconfigure MPU)&lt;/P&gt;&lt;P&gt;Is there a place in SDK configuration where I can select which files will be updated, a part from Update code that does not lists the files above?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Wed, 31 Jan 2024 07:21:27 GMT</pubDate>
    <dc:creator>Amoro</dc:creator>
    <dc:date>2024-01-31T07:21:27Z</dc:date>
    <item>
      <title>XIP folder files undesired update using Configuration Tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1793874#M9475</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am developing an application on a custom MiMXRT1052 board - based on the EVB - with external QSPI flash as code program memory. After a lot of troubles I have been able to make it working, I made a lot of tunings on the code, and one of the key points was to change the "evkbimxrt1050_flexspi_nor_config.c" file in the XIP folder and to re-organize the flexRAM default configuration.&lt;/P&gt;&lt;P&gt;Now everytime I use the MEX Configuration Tool, adding a SDK driver, it changes to default all the modifications I made, and this is really annoying. For example:&lt;/P&gt;&lt;P&gt;- "board.c" is changed without asking enything&lt;/P&gt;&lt;P&gt;- XIP folder files are updated&lt;/P&gt;&lt;P&gt;- StartUpcode.c is updated&lt;/P&gt;&lt;P&gt;erasing every modification I need. Is there a way to avoid this? A special comment sequence to protect the changes in the code?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;AMoro&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jan 2024 14:18:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1793874#M9475</guid>
      <dc:creator>Amoro</dc:creator>
      <dc:date>2024-01-23T14:18:49Z</dc:date>
    </item>
    <item>
      <title>Re: XIP folder files undesired update using Configuration Tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1794119#M9476</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please confirm the following?&lt;/P&gt;
&lt;P&gt;You have your project that already runs XIP correctly in your custom board. And you also have one MEX file with the configuration for peripherals, clocks, pins, etc. And when you want to use that MEX file with the project with the XIP running, it overrides the changes you made in some files. Is this correct?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jan 2024 21:53:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1794119#M9476</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-01-23T21:53:50Z</dc:date>
    </item>
    <item>
      <title>Re: XIP folder files undesired update using Configuration Tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1794750#M9477</link>
      <description>&lt;P&gt;Yes, I confirm. Any idea?&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jan 2024 16:15:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1794750#M9477</guid>
      <dc:creator>Amoro</dc:creator>
      <dc:date>2024-01-24T16:15:51Z</dc:date>
    </item>
    <item>
      <title>Re: XIP folder files undesired update using Configuration Tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1794932#M9478</link>
      <description>When you add a new peripheral using ConfigTools, you will see an&amp;nbsp;Update Code&amp;nbsp;button.&lt;BR /&gt;&lt;BR /&gt;If you click on it, you can see which files are going to be updated, and you can just uncheck the box to avoid the code to be updated, or you can compare the original file with the new one.&lt;BR /&gt;&lt;BR /&gt;I modified the&amp;nbsp;evkbimxrt1050_flexspi_nor_config.c file and then I added new drivers to the project using the "Manage SDK Components" button and I didn't see a change in this file. Could you please tell me what is the driver that is causing the tool to modify these files?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;&lt;BR /&gt;Daniel.</description>
      <pubDate>Wed, 24 Jan 2024 22:44:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1794932#M9478</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-01-24T22:44:07Z</dc:date>
    </item>
    <item>
      <title>Re: XIP folder files undesired update using Configuration Tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1795438#M9479</link>
      <description>&lt;P&gt;Thank you for your answer!&lt;/P&gt;&lt;P&gt;Yes, I know that, but:&lt;/P&gt;&lt;P&gt;- board.c is updated without the possibility to disable the update&lt;/P&gt;&lt;P&gt;- XIP folder the same.&lt;/P&gt;&lt;P&gt;I have enclosed a screen registration, so you can see. It is a ".rar" becouse of dimensions&lt;/P&gt;&lt;P&gt;Andrea&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jan 2024 13:15:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1795438#M9479</guid>
      <dc:creator>Amoro</dc:creator>
      <dc:date>2024-01-25T13:15:03Z</dc:date>
    </item>
    <item>
      <title>Re: XIP folder files undesired update using Configuration Tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1798073#M9488</link>
      <description>&lt;P&gt;If my understanding is correct, the mex file was created under a different project.&lt;/P&gt;
&lt;P&gt;Could you please try to create a new one for this project?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jan 2024 22:16:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1798073#M9488</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-01-30T22:16:48Z</dc:date>
    </item>
    <item>
      <title>Re: XIP folder files undesired update using Configuration Tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1798409#M9489</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;thank you for your answer.&lt;/P&gt;&lt;P&gt;I have regenerated the MEX file for my project but - again - every time I add a new component from SDK all the files are updated:&lt;/P&gt;&lt;P&gt;- XIP folder files.&lt;/P&gt;&lt;P&gt;- startup.c (I relocate flexRAM, so I added modifications to startup_mimxrt1052.c)&lt;/P&gt;&lt;P&gt;- board.c (I relocate flexRAM, so I have to reconfigure MPU)&lt;/P&gt;&lt;P&gt;Is there a place in SDK configuration where I can select which files will be updated, a part from Update code that does not lists the files above?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 07:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1798409#M9489</guid>
      <dc:creator>Amoro</dc:creator>
      <dc:date>2024-01-31T07:21:27Z</dc:date>
    </item>
    <item>
      <title>Re: XIP folder files undesired update using Configuration Tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1799080#M9492</link>
      <description>&lt;P&gt;I don't understand why you are facing this.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What SDK version are you using?&lt;/P&gt;
&lt;P&gt;I added the LCDIF peripheral using Config Tools and the files&amp;nbsp;&lt;EM&gt;board.c &lt;/EM&gt;or &lt;EM&gt;evkbimxrt1050_flexspi_nor_config&lt;/EM&gt;&amp;nbsp;are not being modified (I previously modified these files).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;These are the steps I tried. Please try to replicate this with the latest SDK version 2.15.000:&lt;/P&gt;
&lt;P&gt;- Imported a hello world example&lt;/P&gt;
&lt;P&gt;- Modified the files&lt;/P&gt;
&lt;P&gt;- Imported LCDIF using this button&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DanielRuvalcaba_0-1706737118100.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/261163i6BE85E35A10B047A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="DanielRuvalcaba_0-1706737118100.png" alt="DanielRuvalcaba_0-1706737118100.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;DanielRuvalcaba_0-1706737118100.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;- I pressed Update Code button&lt;/P&gt;
&lt;P&gt;- Compile and verify if the changes still in the files&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 21:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/XIP-folder-files-undesired-update-using-Configuration-Tool/m-p/1799080#M9492</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-01-31T21:42:21Z</dc:date>
    </item>
  </channel>
</rss>