<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: MIMXRT1064 flash tool</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1797095#M9485</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Libor,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We can refer to NXP EVK for this conversation (should be similar), however we may not have a physical access to USB1/UART1/SPI for that purpose. The only thing available for that is JTAG for sure. In that case what kind tool available for that?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;</description>
    <pubDate>Mon, 29 Jan 2024 19:05:12 GMT</pubDate>
    <dc:creator>max_yang1</dc:creator>
    <dc:date>2024-01-29T19:05:12Z</dc:date>
    <item>
      <title>MIMXRT1064 flash tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1795654#M9480</link>
      <description>&lt;P&gt;Is there a standalone&lt;SPAN&gt;&amp;nbsp;flash tool that can program the MIMXRT1064 internal flash outside of IDE?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Max&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jan 2024 21:35:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1795654#M9480</guid>
      <dc:creator>max_yang1</dc:creator>
      <dc:date>2024-01-25T21:35:56Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1064 flash tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1795921#M9481</link>
      <description>&lt;P&gt;Hello Max,&lt;/P&gt;
&lt;P&gt;there's a Secure Provisioning Tool supporting your use case (MIMXRT1064). See here &lt;A href="https://www.nxp.com/mcuxpresso/secure" target="_blank"&gt;https://www.nxp.com/mcuxpresso/secure&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There's also a community for this tool - here &lt;A href="https://community.nxp.com/community/mcuxpresso/mcuxpresso-secure-provisioning-tool" target="_blank"&gt;https://community.nxp.com/community/mcuxpresso/mcuxpresso-secure-provisioning-tool&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Libor&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jan 2024 08:23:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1795921#M9481</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2024-01-26T08:23:36Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1064 flash tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1796936#M9483</link>
      <description>&lt;P&gt;Libor,&lt;/P&gt;&lt;P&gt;Thanks for the links.&lt;/P&gt;&lt;P&gt;Saw this on features of the tool&lt;/P&gt;&lt;P&gt;"Support target connectivity via UART, USB-HID, SPI, and I2C serial download modes"&lt;/P&gt;&lt;P&gt;Not sure on the target connections. I have USB/JTAG probe to the processor. Which type does it covered?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jan 2024 15:01:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1796936#M9483</guid>
      <dc:creator>max_yang1</dc:creator>
      <dc:date>2024-01-29T15:01:42Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1064 flash tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1797038#M9484</link>
      <description>&lt;P&gt;Hi Max,&lt;/P&gt;
&lt;P&gt;SEC tool does not use JTAG, SEC tools talks directly with the Serial Downloader implemented in the device ROM. I do not know what HW you use - your proprietary or still NXP EVK?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If proprietary then you need to look to the Reference Manual (if link works, it should be accessible from here &lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-mcus/i-mx-rt1064-crossover-mcu-with-arm-cortex-m7:i.MX-RT1064" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-mcus/i-mx-rt1064-crossover-mcu-with-arm-cortex-m7:i.MX-RT1064&lt;/A&gt;)&lt;/P&gt;
&lt;P&gt;then look to the chapter 9 System Boot - in short the device must start ISP - using either GPIO pins or fuses and then communicate with ROM via USB1 or LPUART1, see here&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="liborukropec_0-1706548275564.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/260591i6CC5265DD567A0E1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="liborukropec_0-1706548275564.png" alt="liborukropec_0-1706548275564.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;More details can be found in the mentioned RM. IMHO the problem less should be the serial communication with proper USB to serial converter with proper voltage levels.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Libor&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jan 2024 17:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1797038#M9484</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2024-01-29T17:13:02Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1064 flash tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1797095#M9485</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Libor,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We can refer to NXP EVK for this conversation (should be similar), however we may not have a physical access to USB1/UART1/SPI for that purpose. The only thing available for that is JTAG for sure. In that case what kind tool available for that?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jan 2024 19:05:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1797095#M9485</guid>
      <dc:creator>max_yang1</dc:creator>
      <dc:date>2024-01-29T19:05:12Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1064 flash tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1797475#M9486</link>
      <description>&lt;P&gt;Hi Max,&lt;/P&gt;
&lt;P&gt;I'm afraid I'm aware only about GUI Flash tool inside IDE, and then the stand-alone Secure Provisioning Tool.&lt;/P&gt;
&lt;P&gt;Libor&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jan 2024 06:57:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MIMXRT1064-flash-tool/m-p/1797475#M9486</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2024-01-30T06:57:37Z</dc:date>
    </item>
  </channel>
</rss>