<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: Source code of MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Source-code-of-MCUXpresso-IDE/m-p/1785997#M9437</link>
    <description>&lt;P&gt;My understanding is that you're asking for source code associated with the EGit plugins available inside the MCUXpresso IDE. That should not be difficult to find - see&amp;nbsp;&lt;A href="https://git.eclipse.org/" target="_blank"&gt;https://git.eclipse.org/r/plugins/gitiles/egit/egit&lt;/A&gt;&amp;nbsp;or/and&amp;nbsp;&lt;A href="https://github.com/eclipse-egit" target="_blank"&gt;https://github.com/eclipse-egit&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Note that Eclipse-related source code is mostly open-source (EPL licensed) and can be easily inspected by browsing specific repositories. However, MCUXpresso-specific components are based on proprietary source code.&lt;/P&gt;
&lt;P&gt;Not sure about the actual limitations you met but I suggest you switch to the latest MCUXpresso IDE (v11.8.1 available, v11.9.0 to be announced soon) that also comes with newer EGit plugins.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;MCUXpresso IDE Support&lt;/P&gt;</description>
    <pubDate>Wed, 10 Jan 2024 10:10:45 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2024-01-10T10:10:45Z</dc:date>
    <item>
      <title>Source code of MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Source-code-of-MCUXpresso-IDE/m-p/1781341#M9414</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I am using&amp;nbsp;MCUXpresso IDE 11.0.0, I would like to ask if there is a way to reach the source code of it ?&lt;BR /&gt;&lt;BR /&gt;I am working with GIT system that doesn't allow to upload binary files !&lt;BR /&gt;I am thinking to upload the source code, then to compile and then to use !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jan 2024 13:05:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Source-code-of-MCUXpresso-IDE/m-p/1781341#M9414</guid>
      <dc:creator>Mahajna</dc:creator>
      <dc:date>2024-01-01T13:05:10Z</dc:date>
    </item>
    <item>
      <title>Re: Source code of MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Source-code-of-MCUXpresso-IDE/m-p/1781894#M9416</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227628"&gt;@Mahajna&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do you asked how to use git with MCUXpresso IDE?&lt;/P&gt;
&lt;P&gt;If yes, you can refer to EGit User Guider, open from MCUXpresso IDE as below:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1704248075248.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/256413i12D9D7AE21A227A2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1704248075248.png" alt="Alice_Yang_0-1704248075248.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_0-1704248075248.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jan 2024 02:14:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Source-code-of-MCUXpresso-IDE/m-p/1781894#M9416</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-01-03T02:14:53Z</dc:date>
    </item>
    <item>
      <title>Re: Source code of MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Source-code-of-MCUXpresso-IDE/m-p/1782205#M9417</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/27788"&gt;@Alice_Yang&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thank you for your reply&lt;BR /&gt;&lt;BR /&gt;This is not what I meant, I asked if there is any way to get the source code of&amp;nbsp;MCUXpresso IDE ?&lt;BR /&gt;In other words, is&amp;nbsp;MCUXpresso IDE an open source ?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jan 2024 09:34:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Source-code-of-MCUXpresso-IDE/m-p/1782205#M9417</guid>
      <dc:creator>Mahajna</dc:creator>
      <dc:date>2024-01-03T09:34:04Z</dc:date>
    </item>
    <item>
      <title>Re: Source code of MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Source-code-of-MCUXpresso-IDE/m-p/1782639#M9419</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227628"&gt;@Mahajna&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry, no.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jan 2024 03:40:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Source-code-of-MCUXpresso-IDE/m-p/1782639#M9419</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-01-04T03:40:03Z</dc:date>
    </item>
    <item>
      <title>Re: Source code of MCUXpresso IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Source-code-of-MCUXpresso-IDE/m-p/1785997#M9437</link>
      <description>&lt;P&gt;My understanding is that you're asking for source code associated with the EGit plugins available inside the MCUXpresso IDE. That should not be difficult to find - see&amp;nbsp;&lt;A href="https://git.eclipse.org/" target="_blank"&gt;https://git.eclipse.org/r/plugins/gitiles/egit/egit&lt;/A&gt;&amp;nbsp;or/and&amp;nbsp;&lt;A href="https://github.com/eclipse-egit" target="_blank"&gt;https://github.com/eclipse-egit&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Note that Eclipse-related source code is mostly open-source (EPL licensed) and can be easily inspected by browsing specific repositories. However, MCUXpresso-specific components are based on proprietary source code.&lt;/P&gt;
&lt;P&gt;Not sure about the actual limitations you met but I suggest you switch to the latest MCUXpresso IDE (v11.8.1 available, v11.9.0 to be announced soon) that also comes with newer EGit plugins.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;MCUXpresso IDE Support&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jan 2024 10:10:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Source-code-of-MCUXpresso-IDE/m-p/1785997#M9437</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2024-01-10T10:10:45Z</dc:date>
    </item>
  </channel>
</rss>