<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Project dependency in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Project-dependency/m-p/707190#M941</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Erich, that was what I needed.&amp;nbsp; It was the adding the lib objects to the miscellaneous objects in the linker settings that did the trick.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Sep 2017 12:15:07 GMT</pubDate>
    <dc:creator>davidsherman</dc:creator>
    <dc:date>2017-09-20T12:15:07Z</dc:date>
    <item>
      <title>Project dependency</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Project-dependency/m-p/707188#M939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is probably a very basic question, and forgive me since Google isn't coming up with what I'm looking for.&amp;nbsp; I'm migrating a project from KDS to MCUXpresso.&amp;nbsp; Many moons ago, I had dependencies working so if a library was rebuilt because of a source change, the main project would be rebuilt to link in the new library.&amp;nbsp; I've set up the projects with the same hierarchy I had in KDS.&amp;nbsp; The main project links in the libraries generated, and has those projects are listed in "project references".&amp;nbsp; It builds the individual libraries OK if I modify a source, but it doesn't automatically rebuild the main.&amp;nbsp; What was the trick to make it aware that the main depends on the others?&amp;nbsp; I've compared settings in KDS, and it appears I have the same settings, but I must be missing something.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29224iEB3A1E87833E5B77/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 20:12:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Project-dependency/m-p/707188#M939</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2017-09-18T20:12:44Z</dc:date>
    </item>
    <item>
      <title>Re: Project dependency</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Project-dependency/m-p/707189#M940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;maybe &lt;A class="link-titled" href="https://mcuoneclipse.com/2017/09/19/managing-project-and-library-dependencies-with-eclipse-cdt/" title="https://mcuoneclipse.com/2017/09/19/managing-project-and-library-dependencies-with-eclipse-cdt/"&gt;Managing Project and Library Dependencies with Eclipse CDT | MCU on Eclipse&lt;/A&gt;&amp;nbsp; is what you are looking for?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Sep 2017 20:23:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Project-dependency/m-p/707189#M940</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-09-19T20:23:19Z</dc:date>
    </item>
    <item>
      <title>Re: Project dependency</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Project-dependency/m-p/707190#M941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Erich, that was what I needed.&amp;nbsp; It was the adding the lib objects to the miscellaneous objects in the linker settings that did the trick.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2017 12:15:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Project-dependency/m-p/707190#M941</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2017-09-20T12:15:07Z</dc:date>
    </item>
  </channel>
</rss>