<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: Cannot create a launch configuration</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-create-a-launch-configuration/m-p/1771107#M9362</link>
    <description>&lt;P&gt;Hello, I found a similar thread I suggest following the steps mentioned on this.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE/The-launch-configuration-blah-Debug-is-incompatible-with-this/m-p/1330417#M7336" target="_blank"&gt;Solved: The launch configuration 'blah Debug' is incompati... - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Could you elaborate further on these questions, I saw on the image you have a K81, is this a custom board or EVK? On the same image have the configuration for the J-Link, are you using an external debugger or the debugger on the board?&lt;/P&gt;
&lt;P&gt;When you import the project on the 11.4 the launch configuration was created by you or by the tool? I mean the bug blue or green. did you erase the debug file? Did you clean the project and refresh it? Did you erase the old launch configuration?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
    <pubDate>Thu, 07 Dec 2023 22:27:58 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2023-12-07T22:27:58Z</dc:date>
    <item>
      <title>Cannot create a launch configuration</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-create-a-launch-configuration/m-p/1769059#M9353</link>
      <description>&lt;P&gt;We were running with the latest 11.8 version of MCUXpresso but needed to revert to 11.4.1 to have a particular version of GCC.&amp;nbsp; I was able to install it into a new directory and import and build the projects without any problems, but now that I want to set up a launch configuration, it gives a series of error messages that I cannot get past.&lt;BR /&gt;&lt;BR /&gt;"The launch configuration 'xxx my project name xxx' is incompatible with this version of MCUXpresso IDE.&amp;nbsp;Migrate the launch configuration to the supported format?&lt;/P&gt;&lt;P&gt;If I say 'yes', it says 'Deprecated launch configuration attributes will not be migrated to the new attributes; the new attributes will be set to their default values!"&lt;/P&gt;&lt;P&gt;It then gives me the normal dialog where I can fill out details.&amp;nbsp; When I select 'Debug' it gives me the same message as above that its incompatible and asks to migrate the configuration.&amp;nbsp; Then it says that it could not be migrated and should be deleted.&lt;BR /&gt;&lt;BR /&gt;It's an endless cycle.&amp;nbsp; First, I never supplied a launch config in the first place and would be happy to create a new one but there seems to be no way to do that. Second, there is no way out of this endless cycle.&amp;nbsp; I have tried deleting any config that I can find, but it keeps coming back and pretending that I have already set it up and it needs to be migrated, etc.&lt;/P&gt;&lt;P&gt;When I installed version 11.4, I put it in its own directory, so it should not be finding launch config files from the 11.8 version.&amp;nbsp; So, I have no idea what is happening.&lt;BR /&gt;&lt;BR /&gt;Additionally, the 'Debug' button is almost always grayed out, but when its not grayed out, if I click it, I get the error messages described above.&amp;nbsp; How is it that I should have to migrate a launch configuration that I just created?&lt;/P&gt;</description>
      <pubDate>Tue, 05 Dec 2023 14:01:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-create-a-launch-configuration/m-p/1769059#M9353</guid>
      <dc:creator>RogerDavisWork</dc:creator>
      <dc:date>2023-12-05T14:01:01Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot create a launch configuration</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-create-a-launch-configuration/m-p/1769301#M9355</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I found the release notes of the IDE v11.8 and 11.8.11 and I found the version of the GCC below.&lt;/P&gt;
&lt;UL type="disc"&gt;
&lt;LI&gt;&lt;SPAN&gt;Upgraded: GNU ARM Embedded Toolchain to version 12.2.Rel1.&lt;/SPAN&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE-Knowledge-Base/MCUXpresso-IDE-v11-8-1-Now-Available/ta-p/1750344" target="_blank"&gt;MCUXpresso IDE v11.8.1 Now Available - NXP Community&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE-Knowledge-Base/MCUXpresso-IDE-v11-8-0-Now-Available/ta-p/1696945" target="_blank"&gt;MCUXpresso IDE v11.8.0 Now Available - NXP Community&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;But I can find&amp;nbsp;the version of the GCC on the 11.4&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE-Knowledge-Base/MCUXpresso-IDE-Release-History/ta-p/1113669" target="_blank"&gt;MCUXpresso IDE - Release History - NXP Community&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;What is the version do you need?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 05 Dec 2023 22:10:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-create-a-launch-configuration/m-p/1769301#M9355</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-12-05T22:10:08Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot create a launch configuration</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-create-a-launch-configuration/m-p/1769796#M9356</link>
      <description>&lt;P&gt;I don't need a version of MCUXpresso. As my question says, I downloaded 11.4.1 and have been able to import and build my projects.&amp;nbsp; The issue that I am having is that it will not let me create a launch configuration. When I try to create one, it always says that it does not support the format and it needs to migrate it to the new version.&amp;nbsp; But, this is a launch configuration that IT CREATED, so why does it think that it needs to migrate the version?&amp;nbsp; Additionally, when I agree and let it migrate it, it says that it failed and tells me to delete the launch configuration.&amp;nbsp; I can only guess that it is confused because I have two versions of MCUXpresso on my computer and maybe that is confusing it.&amp;nbsp; I can still create and use launch configurations for the 11.8 version, just not the 11.4 version.&amp;nbsp; I believe this is a bug somehow and have no way to fix it.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Dec 2023 13:27:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-create-a-launch-configuration/m-p/1769796#M9356</guid>
      <dc:creator>RogerDavisWork</dc:creator>
      <dc:date>2023-12-06T13:27:36Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot create a launch configuration</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-create-a-launch-configuration/m-p/1771107#M9362</link>
      <description>&lt;P&gt;Hello, I found a similar thread I suggest following the steps mentioned on this.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE/The-launch-configuration-blah-Debug-is-incompatible-with-this/m-p/1330417#M7336" target="_blank"&gt;Solved: The launch configuration 'blah Debug' is incompati... - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Could you elaborate further on these questions, I saw on the image you have a K81, is this a custom board or EVK? On the same image have the configuration for the J-Link, are you using an external debugger or the debugger on the board?&lt;/P&gt;
&lt;P&gt;When you import the project on the 11.4 the launch configuration was created by you or by the tool? I mean the bug blue or green. did you erase the debug file? Did you clean the project and refresh it? Did you erase the old launch configuration?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 07 Dec 2023 22:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-create-a-launch-configuration/m-p/1771107#M9362</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-12-07T22:27:58Z</dc:date>
    </item>
  </channel>
</rss>