<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Starting debugger using MCUXpresso fails under Debian in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Starting-debugger-using-MCUXpresso-fails-under-Debian/m-p/1747999#M9254</link>
    <description>&lt;P&gt;IDE: MCUXpresso v11.8.0&lt;/P&gt;&lt;P&gt;SDK: SDK_2_14_0_MIMXRT1170-EVKB-LINUX&lt;/P&gt;&lt;P&gt;Target board: MIMXRT1170-EVKB&lt;/P&gt;&lt;P&gt;Trying debug an m7 project fails with the message: 'Launching m7 LinkServer Debug' has encountered a problem, problem file does not exist. The file path to the binary is "m7/Debug\m7.axf", which contains an error as it contains a "\" instead of "/". The build is successful, the board is detected and the file does "m7/debug/m7.axf" exists.&lt;/P&gt;&lt;P&gt;Any way to fix this?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Fri, 27 Oct 2023 18:57:24 GMT</pubDate>
    <dc:creator>achampoux</dc:creator>
    <dc:date>2023-10-27T18:57:24Z</dc:date>
    <item>
      <title>Starting debugger using MCUXpresso fails under Debian</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Starting-debugger-using-MCUXpresso-fails-under-Debian/m-p/1747999#M9254</link>
      <description>&lt;P&gt;IDE: MCUXpresso v11.8.0&lt;/P&gt;&lt;P&gt;SDK: SDK_2_14_0_MIMXRT1170-EVKB-LINUX&lt;/P&gt;&lt;P&gt;Target board: MIMXRT1170-EVKB&lt;/P&gt;&lt;P&gt;Trying debug an m7 project fails with the message: 'Launching m7 LinkServer Debug' has encountered a problem, problem file does not exist. The file path to the binary is "m7/Debug\m7.axf", which contains an error as it contains a "\" instead of "/". The build is successful, the board is detected and the file does "m7/debug/m7.axf" exists.&lt;/P&gt;&lt;P&gt;Any way to fix this?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 27 Oct 2023 18:57:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Starting-debugger-using-MCUXpresso-fails-under-Debian/m-p/1747999#M9254</guid>
      <dc:creator>achampoux</dc:creator>
      <dc:date>2023-10-27T18:57:24Z</dc:date>
    </item>
    <item>
      <title>Re: Starting debugger using MCUXpresso fails under Debian</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Starting-debugger-using-MCUXpresso-fails-under-Debian/m-p/1749289#M9257</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224961"&gt;@achampoux&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;How about first debug a SDK demo without any change?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 31 Oct 2023 07:53:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Starting-debugger-using-MCUXpresso-fails-under-Debian/m-p/1749289#M9257</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-10-31T07:53:24Z</dc:date>
    </item>
  </channel>
</rss>