<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Implement MS OS descriptor functionality in virtual printer bm example</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Implement-MS-OS-descriptor-functionality-in-virtual-printer-bm/m-p/1715269#M9151</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;We are trying to use the virtual printer bm example specifically : lpcexpresso_54s018_dev_printer_virtual_plain_text_bm example.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have the basic functionality working, but need to add MS OS descriptor functionality so that the USB device registers as a WinUSB and therefore no driver signing is necessary.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are seeing Windows request the stringDescriptor at index 0xEE. We are having trouble getting Windows to request the other two needed descriptors. Specifically :&lt;/P&gt;&lt;P&gt;the&amp;nbsp;WINUSB_ExtendedCompatId Descriptor&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;the&amp;nbsp;WINUSB_ExtendedProperty_InterfaceGUID_Descriptor&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to provide some help/guidance on how we can get Windows to request these two descriptors using the previously mentioned example as a starting point&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Victor&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 31 Aug 2023 17:02:01 GMT</pubDate>
    <dc:creator>shabaka101694</dc:creator>
    <dc:date>2023-08-31T17:02:01Z</dc:date>
    <item>
      <title>Implement MS OS descriptor functionality in virtual printer bm example</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Implement-MS-OS-descriptor-functionality-in-virtual-printer-bm/m-p/1715269#M9151</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;We are trying to use the virtual printer bm example specifically : lpcexpresso_54s018_dev_printer_virtual_plain_text_bm example.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have the basic functionality working, but need to add MS OS descriptor functionality so that the USB device registers as a WinUSB and therefore no driver signing is necessary.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are seeing Windows request the stringDescriptor at index 0xEE. We are having trouble getting Windows to request the other two needed descriptors. Specifically :&lt;/P&gt;&lt;P&gt;the&amp;nbsp;WINUSB_ExtendedCompatId Descriptor&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;the&amp;nbsp;WINUSB_ExtendedProperty_InterfaceGUID_Descriptor&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to provide some help/guidance on how we can get Windows to request these two descriptors using the previously mentioned example as a starting point&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Victor&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Aug 2023 17:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Implement-MS-OS-descriptor-functionality-in-virtual-printer-bm/m-p/1715269#M9151</guid>
      <dc:creator>shabaka101694</dc:creator>
      <dc:date>2023-08-31T17:02:01Z</dc:date>
    </item>
    <item>
      <title>Re: Implement MS OS descriptor functionality in virtual printer bm example</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Implement-MS-OS-descriptor-functionality-in-virtual-printer-bm/m-p/1715453#M9152</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Regarding the question about&amp;nbsp; MS OS descriptor functionality in virtual printer bm example, I have asked AE team, I will answer you after I get response.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 01 Sep 2023 02:18:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Implement-MS-OS-descriptor-functionality-in-virtual-printer-bm/m-p/1715453#M9152</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-09-01T02:18:38Z</dc:date>
    </item>
    <item>
      <title>Re: Implement MS OS descriptor functionality in virtual printer bm example</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Implement-MS-OS-descriptor-functionality-in-virtual-printer-bm/m-p/1721828#M9169</link>
      <description>&lt;P&gt;hi，&lt;SPAN&gt;shabaka101694&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;You can refer to this question and answer, hope it will help you.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-General/LPC54S018-WinUSB-driver-signing/td-p/1703179" target="_blank"&gt;https://community.nxp.com/t5/MCUXpresso-General/LPC54S018-WinUSB-driver-signing/td-p/1703179&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Xu Zhang&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 08:01:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Implement-MS-OS-descriptor-functionality-in-virtual-printer-bm/m-p/1721828#M9169</guid>
      <dc:creator>Xu_Zhang</dc:creator>
      <dc:date>2023-09-13T08:01:34Z</dc:date>
    </item>
  </channel>
</rss>