<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックXRT1160/1170 Software reset</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/XRT1160-1170-Software-reset/m-p/1708538#M9132</link>
    <description>&lt;P&gt;I am trying to reset the XRT1160/1170 via software. I have tried a few methods and all have failed&lt;/P&gt;&lt;P&gt;What I have tried so far:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;NVIC_SystemReset();&lt;/LI&gt;&lt;LI&gt;WDOG_TriggerSystemSoftwareReset(WDOG);&lt;/LI&gt;&lt;LI&gt;wdog_config_t config;&lt;BR /&gt;WDOG_GetDefaultConfig(&amp;amp;config);&lt;BR /&gt;config.timeoutValue = 0xFU; /* Timeout value is (0xF+1)/2 = 8 sec. */&lt;BR /&gt;WDOG_Init(WDOG1, &amp;amp;config)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;All of them hang the MCU, debugging stops, and it doesn't complete the reset.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is on a custom board with an IS25xxx QSPI Chip&amp;nbsp;&lt;A href="https://www.issi.com/WW/pdf/flash-spi_electronica2014.pdf" target="_blank"&gt;https://www.issi.com/WW/pdf/flash-spi_electronica2014.pdf&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Along with the above mentioned attempts I have read through multiple other blog posts to no avail. I have also tried the watchdog example and the reset example, neither correctly reset the MCU.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Cole&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 21 Aug 2023 19:20:42 GMT</pubDate>
    <dc:creator>csutyaksancsoft</dc:creator>
    <dc:date>2023-08-21T19:20:42Z</dc:date>
    <item>
      <title>XRT1160/1170 Software reset</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/XRT1160-1170-Software-reset/m-p/1708538#M9132</link>
      <description>&lt;P&gt;I am trying to reset the XRT1160/1170 via software. I have tried a few methods and all have failed&lt;/P&gt;&lt;P&gt;What I have tried so far:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;NVIC_SystemReset();&lt;/LI&gt;&lt;LI&gt;WDOG_TriggerSystemSoftwareReset(WDOG);&lt;/LI&gt;&lt;LI&gt;wdog_config_t config;&lt;BR /&gt;WDOG_GetDefaultConfig(&amp;amp;config);&lt;BR /&gt;config.timeoutValue = 0xFU; /* Timeout value is (0xF+1)/2 = 8 sec. */&lt;BR /&gt;WDOG_Init(WDOG1, &amp;amp;config)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;All of them hang the MCU, debugging stops, and it doesn't complete the reset.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is on a custom board with an IS25xxx QSPI Chip&amp;nbsp;&lt;A href="https://www.issi.com/WW/pdf/flash-spi_electronica2014.pdf" target="_blank"&gt;https://www.issi.com/WW/pdf/flash-spi_electronica2014.pdf&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Along with the above mentioned attempts I have read through multiple other blog posts to no avail. I have also tried the watchdog example and the reset example, neither correctly reset the MCU.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Cole&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 19:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/XRT1160-1170-Software-reset/m-p/1708538#M9132</guid>
      <dc:creator>csutyaksancsoft</dc:creator>
      <dc:date>2023-08-21T19:20:42Z</dc:date>
    </item>
    <item>
      <title>Re: XRT1160/1170 Software reset</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/XRT1160-1170-Software-reset/m-p/1708546#M9133</link>
      <description>&lt;P&gt;I figured it out, the debugger was halting the code. If I disconnect&amp;nbsp; the Debugger it works as intended.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;specifically&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;wdog_config_t config;&lt;BR /&gt;WDOG_GetDefaultConfig(&amp;amp;config);&lt;BR /&gt;config.timeoutValue = 0xFU; /* Timeout value is (0xF+1)/2 = 8 sec. */&lt;BR /&gt;WDOG_Init(WDOG1, &amp;amp;config)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Works&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 19:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/XRT1160-1170-Software-reset/m-p/1708546#M9133</guid>
      <dc:creator>csutyaksancsoft</dc:creator>
      <dc:date>2023-08-21T19:36:03Z</dc:date>
    </item>
  </channel>
</rss>