<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to know which SDK components to include? in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-know-which-SDK-components-to-include/m-p/1669460#M9042</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182695"&gt;@simmania&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;When you select the board and click on build sdk, the minimum files for the sdk to work are selected by default, unless you need one of the other options you can add it. Also, there is a description for each option. In case you want to have all the options for development you can select all of them but this depends on the target.&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;</description>
    <pubDate>Wed, 14 Jun 2023 16:44:54 GMT</pubDate>
    <dc:creator>Miguel04</dc:creator>
    <dc:date>2023-06-14T16:44:54Z</dc:date>
    <item>
      <title>How to know which SDK components to include?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-know-which-SDK-components-to-include/m-p/1668543#M9038</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I'm new to MCUXpresso and the tools. I have a hard time understanding how to know what to include in the SDK when building the SDK.&lt;BR /&gt;&lt;BR /&gt;For instance the &lt;STRONG&gt;Drivers&lt;/STRONG&gt;:&lt;BR /&gt;&lt;BR /&gt;We understand you need to add the SAI Driver when you want to use the SAI peripheral. But there are many drivers from which it is not clear if we should add them. The most basic demos include for instance drivers like:&lt;BR /&gt;CACHE Driver&lt;BR /&gt;Clock Driver&lt;BR /&gt;COMMON Driver&lt;BR /&gt;DCDC SOC Driver&lt;BR /&gt;PMU Driver&lt;BR /&gt;XIP Device Driver&lt;/P&gt;&lt;P&gt;How do I know which I need to include? How can I find a description of these drivers?&lt;/P&gt;&lt;P&gt;And about the &lt;STRONG&gt;CMSIS Include&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;Most demos include the&lt;BR /&gt;CMSIS_Include_CM&lt;BR /&gt;MIMXRT1176_CMSIS&lt;BR /&gt;MIMXRT1176_system&lt;BR /&gt;What are they and do I always need to include them?&lt;/P&gt;&lt;P&gt;Then there are the &lt;STRONG&gt;Utilities&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;Even the simplest demos include:&lt;BR /&gt;assert&lt;BR /&gt;debug_console (or debug_console_lite)&lt;BR /&gt;lpuart_adapter&lt;BR /&gt;misc_utilities&lt;BR /&gt;serial_manager&lt;BR /&gt;serial_manager_uart&lt;/P&gt;&lt;P&gt;How can we find information what they are to be able to decide if we need them?&lt;/P&gt;&lt;P&gt;And then there is the &lt;STRONG&gt;Middleware&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;How to find out what functinality they add and what the API is to that we can decide if we need it?&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 16:06:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-know-which-SDK-components-to-include/m-p/1668543#M9038</guid>
      <dc:creator>simmania</dc:creator>
      <dc:date>2023-06-13T16:06:02Z</dc:date>
    </item>
    <item>
      <title>Re: How to know which SDK components to include?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-know-which-SDK-components-to-include/m-p/1669460#M9042</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182695"&gt;@simmania&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;When you select the board and click on build sdk, the minimum files for the sdk to work are selected by default, unless you need one of the other options you can add it. Also, there is a description for each option. In case you want to have all the options for development you can select all of them but this depends on the target.&lt;/P&gt;
&lt;P&gt;Best Regards, Miguel.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 16:44:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-know-which-SDK-components-to-include/m-p/1669460#M9042</guid>
      <dc:creator>Miguel04</dc:creator>
      <dc:date>2023-06-14T16:44:54Z</dc:date>
    </item>
    <item>
      <title>Re: How to know which SDK components to include?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-know-which-SDK-components-to-include/m-p/1674328#M9054</link>
      <description>&lt;P&gt;I share your frustration with&amp;nbsp;&lt;A href="https://community.nxp.com/t5/MCUXpresso-SDK/Documentation-of-SDK-components-drivers-middleware-abstraction/m-p/1349217" target="_self"&gt;NXP style documentation&lt;/A&gt;&amp;nbsp;of the SDK API and components. It's partly compensated by this friendly and helpful community &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jun 2023 09:20:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/How-to-know-which-SDK-components-to-include/m-p/1674328#M9054</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2023-06-22T09:20:20Z</dc:date>
    </item>
  </channel>
</rss>