<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic lpc4370 multicore applications in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/lpc4370-multicore-applications/m-p/1662729#M9015</link>
    <description>&lt;P&gt;Is there documentation explaining how the multicore applications work for the lpc4370 processor?&lt;/P&gt;&lt;P&gt;What flash driver files and memory configuration files should be used for multicore applications for the lpc4370 processor?&lt;/P&gt;&lt;P&gt;Is there a guide for using the flash driver files and the memory configuration files for multicore applications for the lpc4370 processor?&lt;/P&gt;&lt;P&gt;Why do I get “error uses VFP register arguments” when running the multicore_blinky examples on the lpc4370 and how do I solve them?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did not get this error when running the multicore_blinky applications on the lpc43S67 processor. I did refer to the LPC43xx Cortex-M4 / M0 Multicore Applications document. In this document, I saw that the M4 application can be placed in Flash A (at 0x1a000000) and the M0APP application can be placed in Flash B. This makes sense when looking at the memory details of the lpc43S67 because there is a flash A and flash B. The memory details of the lpc4370 project do not contain a flash A or flash B. The default Link Server Flash Driver was empty by default, so I tried using the LPC18_43_SPIFI_GENERIC.cfx file for this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone help with this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#&lt;A href="https://community.nxp.com/t5/tag/lpc43xx/tg-p/board-id/lpc" target="_blank" rel="noopener tag"&gt;lpc43xx&lt;/A&gt;&lt;/P&gt;&lt;P&gt;#&lt;A href="https://community.nxp.com/t5/tag/multicore/tg-p/board-id/lpc" target="_blank" rel="noopener tag"&gt;multicore&lt;/A&gt;&lt;/P&gt;&lt;P&gt;#&lt;A href="https://community.nxp.com/t5/tag/flash%20map/tg-p/board-id/lpc" target="_blank" rel="noopener tag"&gt;flash map&lt;/A&gt;&lt;/P&gt;&lt;P&gt;#&lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/lpcopen-libraries-and-examples/lpcopen-software-development-platform-lpc43xx:LPCOPEN-SOFTWARE-FOR-LPC43XX" target="_self"&gt;LPC Open&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 02 Jun 2023 14:40:46 GMT</pubDate>
    <dc:creator>smarty760</dc:creator>
    <dc:date>2023-06-02T14:40:46Z</dc:date>
    <item>
      <title>lpc4370 multicore applications</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/lpc4370-multicore-applications/m-p/1662729#M9015</link>
      <description>&lt;P&gt;Is there documentation explaining how the multicore applications work for the lpc4370 processor?&lt;/P&gt;&lt;P&gt;What flash driver files and memory configuration files should be used for multicore applications for the lpc4370 processor?&lt;/P&gt;&lt;P&gt;Is there a guide for using the flash driver files and the memory configuration files for multicore applications for the lpc4370 processor?&lt;/P&gt;&lt;P&gt;Why do I get “error uses VFP register arguments” when running the multicore_blinky examples on the lpc4370 and how do I solve them?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did not get this error when running the multicore_blinky applications on the lpc43S67 processor. I did refer to the LPC43xx Cortex-M4 / M0 Multicore Applications document. In this document, I saw that the M4 application can be placed in Flash A (at 0x1a000000) and the M0APP application can be placed in Flash B. This makes sense when looking at the memory details of the lpc43S67 because there is a flash A and flash B. The memory details of the lpc4370 project do not contain a flash A or flash B. The default Link Server Flash Driver was empty by default, so I tried using the LPC18_43_SPIFI_GENERIC.cfx file for this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone help with this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#&lt;A href="https://community.nxp.com/t5/tag/lpc43xx/tg-p/board-id/lpc" target="_blank" rel="noopener tag"&gt;lpc43xx&lt;/A&gt;&lt;/P&gt;&lt;P&gt;#&lt;A href="https://community.nxp.com/t5/tag/multicore/tg-p/board-id/lpc" target="_blank" rel="noopener tag"&gt;multicore&lt;/A&gt;&lt;/P&gt;&lt;P&gt;#&lt;A href="https://community.nxp.com/t5/tag/flash%20map/tg-p/board-id/lpc" target="_blank" rel="noopener tag"&gt;flash map&lt;/A&gt;&lt;/P&gt;&lt;P&gt;#&lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/lpcopen-libraries-and-examples/lpcopen-software-development-platform-lpc43xx:LPCOPEN-SOFTWARE-FOR-LPC43XX" target="_self"&gt;LPC Open&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 14:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/lpc4370-multicore-applications/m-p/1662729#M9015</guid>
      <dc:creator>smarty760</dc:creator>
      <dc:date>2023-06-02T14:40:46Z</dc:date>
    </item>
    <item>
      <title>Re: lpc4370 multicore applications</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/lpc4370-multicore-applications/m-p/1663808#M9016</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218278"&gt;@smarty760&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is no internal flash with lpc4370.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;LPC18_43_SPIFI_GENERIC.cfx file&amp;nbsp; is for external spifi flash. you can open demos under LPCopen to check.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;About debug multicore, you can also have a look at thread:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPC-Microcontrollers/Which-IDE-to-be-used-for-debugging-LPC4367/m-p/871786" target="_blank"&gt;https://community.nxp.com/t5/LPC-Microcontrollers/Which-IDE-to-be-used-for-debugging-LPC4367/m-p/871786&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jun 2023 02:49:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/lpc4370-multicore-applications/m-p/1663808#M9016</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-06-06T02:49:21Z</dc:date>
    </item>
  </channel>
</rss>