<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCUXPRESSO overflow SRAM after setup peripheral modules in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXPRESSO-overflow-SRAM-after-setup-peripheral-modules/m-p/1640623#M8923</link>
    <description>&lt;P&gt;Hello Alice.&lt;/P&gt;&lt;P&gt;I figured out the problem (I guess).&amp;nbsp;&lt;/P&gt;&lt;P&gt;As the picture below, the field "Allocate Messages RAM" should not be checked. When it is checked, the SRAM overflows.&lt;/P&gt;&lt;P&gt;Yes, is a issue related to CAN. There are no troubles with another modules.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN_RAM.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220955i8F990662477E7431/image-size/large?v=v2&amp;amp;px=999" role="button" title="CAN_RAM.png" alt="CAN_RAM.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But Alice, let me know. Is possible allocate the messages in the SRAMX or SRAM3 areas?&lt;BR /&gt;&lt;BR /&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Wed, 26 Apr 2023 13:32:47 GMT</pubDate>
    <dc:creator>clkunde</dc:creator>
    <dc:date>2023-04-26T13:32:47Z</dc:date>
    <item>
      <title>MCUXPRESSO overflow SRAM after setup peripheral modules</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXPRESSO-overflow-SRAM-after-setup-peripheral-modules/m-p/1636516#M8914</link>
      <description>&lt;P&gt;Hi Folks!&lt;/P&gt;&lt;P&gt;I'm getting a weird error when I try to change (or enable) some peripheral in my project, after the first setup.&lt;BR /&gt;&lt;BR /&gt;The MCU is LPC55S06JHI48&lt;BR /&gt;The MCUXPRESSO IDE version (was installed today) is&amp;nbsp;v11.7.1 [Build 9221] [2023-03-28]&lt;BR /&gt;The SDK&amp;nbsp; is&amp;nbsp;SDK_2.x_LPC55S06 2.13.0.201911251446&lt;/P&gt;&lt;P&gt;If I start and setup a new project, after compile, I get no errors and the usage of the SRAM is ok, like the figure below.&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mem_ok.png" style="width: 758px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219926i4C46244676D5A41F/image-size/large?v=v2&amp;amp;px=999" role="button" title="mem_ok.png" alt="mem_ok.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But, if I try to modify (disable, enable or insert a new peripheral or drive), the compiler overflow the SRAM. (see the picture below)&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mem_error.png" style="width: 758px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219932i8AAA41F05B94F815/image-size/large?v=v2&amp;amp;px=999" role="button" title="mem_error.png" alt="mem_error.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The next picture is an example that I tried to do. I disable the CAN peripheral to do some tests, but when I enable them, the SRAM overflow happens again.&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="peripheral_enable.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219934i2D429637019CECD2/image-size/large?v=v2&amp;amp;px=999" role="button" title="peripheral_enable.png" alt="peripheral_enable.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is not something related to CAN module. If I try to change RTC, FLEXCOM or any other modulo, I get the same error. The same occurs when some driver is installed on the project, after the first setup.&lt;BR /&gt;&lt;BR /&gt;Maybe it is a bug in a MCUXPRESSO? Somebody got something similar, could me help.&lt;BR /&gt;&lt;BR /&gt;Thank you my friends!&lt;/P&gt;</description>
      <pubDate>Wed, 19 Apr 2023 19:33:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXPRESSO-overflow-SRAM-after-setup-peripheral-modules/m-p/1636516#M8914</guid>
      <dc:creator>clkunde</dc:creator>
      <dc:date>2023-04-19T19:33:15Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXPRESSO overflow SRAM after setup peripheral modules</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXPRESSO-overflow-SRAM-after-setup-peripheral-modules/m-p/1637629#M8917</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/175304"&gt;@clkunde&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please send your project, I help you check on my side, thanks.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 21 Apr 2023 02:55:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXPRESSO-overflow-SRAM-after-setup-peripheral-modules/m-p/1637629#M8917</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-04-21T02:55:02Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXPRESSO overflow SRAM after setup peripheral modules</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXPRESSO-overflow-SRAM-after-setup-peripheral-modules/m-p/1640623#M8923</link>
      <description>&lt;P&gt;Hello Alice.&lt;/P&gt;&lt;P&gt;I figured out the problem (I guess).&amp;nbsp;&lt;/P&gt;&lt;P&gt;As the picture below, the field "Allocate Messages RAM" should not be checked. When it is checked, the SRAM overflows.&lt;/P&gt;&lt;P&gt;Yes, is a issue related to CAN. There are no troubles with another modules.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN_RAM.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/220955i8F990662477E7431/image-size/large?v=v2&amp;amp;px=999" role="button" title="CAN_RAM.png" alt="CAN_RAM.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But Alice, let me know. Is possible allocate the messages in the SRAMX or SRAM3 areas?&lt;BR /&gt;&lt;BR /&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 26 Apr 2023 13:32:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXPRESSO-overflow-SRAM-after-setup-peripheral-modules/m-p/1640623#M8923</guid>
      <dc:creator>clkunde</dc:creator>
      <dc:date>2023-04-26T13:32:47Z</dc:date>
    </item>
  </channel>
</rss>