<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックIs It possible to write a File from controller to PC(Only through Command Line)</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Is-It-possible-to-write-a-File-from-controller-to-PC-Only/m-p/702736#M886</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi MCUXprsso Team, I want to write a file from the controller to PC when MCUXpresso IDE is running and debugger(JLink/Link2) is connected, It is working fine. when I tried to write through command line&amp;nbsp;where NO Ide is alive it is not happening. Is there any way to write into a file from the controller if MCUXpresso is not alive. I have used All commands for flashing and Reset for MCUXpresso only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Chandan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Sep 2017 07:06:39 GMT</pubDate>
    <dc:creator>tosinghchandan</dc:creator>
    <dc:date>2017-09-14T07:06:39Z</dc:date>
    <item>
      <title>Is It possible to write a File from controller to PC(Only through Command Line)</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Is-It-possible-to-write-a-File-from-controller-to-PC-Only/m-p/702736#M886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi MCUXprsso Team, I want to write a file from the controller to PC when MCUXpresso IDE is running and debugger(JLink/Link2) is connected, It is working fine. when I tried to write through command line&amp;nbsp;where NO Ide is alive it is not happening. Is there any way to write into a file from the controller if MCUXpresso is not alive. I have used All commands for flashing and Reset for MCUXpresso only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Chandan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Sep 2017 07:06:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Is-It-possible-to-write-a-File-from-controller-to-PC-Only/m-p/702736#M886</guid>
      <dc:creator>tosinghchandan</dc:creator>
      <dc:date>2017-09-14T07:06:39Z</dc:date>
    </item>
    <item>
      <title>Re: Is It possible to write a File from controller to PC(Only through Command Line)</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Is-It-possible-to-write-a-File-from-controller-to-PC-Only/m-p/702737#M887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No. File I/O from your ARM target application is done by a debugger servicing semihost calls. Without the debugger, there is no service.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Sep 2017 21:18:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Is-It-possible-to-write-a-File-from-controller-to-PC-Only/m-p/702737#M887</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-09-15T21:18:03Z</dc:date>
    </item>
  </channel>
</rss>