<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Setting a breakpoint halts the system in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Setting-a-breakpoint-halts-the-system/m-p/1548994#M8539</link>
    <description>&lt;P&gt;Hi Daan,&lt;/P&gt;&lt;P&gt;How breakpoints are set, depends on your debug probe technology. For example the SEGGER J-Link is very fast and is able to reprogram the flash page with a software breakpoint. However, this kind of things requires the target to be halted, programming the flash and then continue.&lt;/P&gt;&lt;P&gt;The other way is to use hardware breakpoints: but this still requires the target to be halted afik.&lt;/P&gt;&lt;P&gt;For an explanation how breakpoints work, see &lt;A href="https://mcuoneclipse.com/2012/07/29/software-and-hardware-breakpoints/" target="_blank"&gt;https://mcuoneclipse.com/2012/07/29/software-and-hardware-breakpoints/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The only way to get around this is that the debugger is only able to read/write the RAM memory while the target is running, using some bus free cycles. So you would only be able to do this if your code is running in RAM instead of FLASH.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
    <pubDate>Fri, 04 Nov 2022 17:49:53 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2022-11-04T17:49:53Z</dc:date>
    <item>
      <title>Setting a breakpoint halts the system</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Setting-a-breakpoint-halts-the-system/m-p/1548766#M8536</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Whenever my system is running (RT1064 core) and I want to set a breakpoint in runtime, the system halts for a few seconds, after this, normal operation is continued, however, the system has become useless, since other CAN devices missed the heartbeat of the controller. Isn't there a way to set and remove breakpoints transparently?&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Daan&lt;/P&gt;</description>
      <pubDate>Fri, 04 Nov 2022 08:14:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Setting-a-breakpoint-halts-the-system/m-p/1548766#M8536</guid>
      <dc:creator>Daan</dc:creator>
      <dc:date>2022-11-04T08:14:42Z</dc:date>
    </item>
    <item>
      <title>Re: Setting a breakpoint halts the system</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Setting-a-breakpoint-halts-the-system/m-p/1548994#M8539</link>
      <description>&lt;P&gt;Hi Daan,&lt;/P&gt;&lt;P&gt;How breakpoints are set, depends on your debug probe technology. For example the SEGGER J-Link is very fast and is able to reprogram the flash page with a software breakpoint. However, this kind of things requires the target to be halted, programming the flash and then continue.&lt;/P&gt;&lt;P&gt;The other way is to use hardware breakpoints: but this still requires the target to be halted afik.&lt;/P&gt;&lt;P&gt;For an explanation how breakpoints work, see &lt;A href="https://mcuoneclipse.com/2012/07/29/software-and-hardware-breakpoints/" target="_blank"&gt;https://mcuoneclipse.com/2012/07/29/software-and-hardware-breakpoints/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The only way to get around this is that the debugger is only able to read/write the RAM memory while the target is running, using some bus free cycles. So you would only be able to do this if your code is running in RAM instead of FLASH.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Fri, 04 Nov 2022 17:49:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Setting-a-breakpoint-halts-the-system/m-p/1548994#M8539</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2022-11-04T17:49:53Z</dc:date>
    </item>
    <item>
      <title>Re: Setting a breakpoint halts the system</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Setting-a-breakpoint-halts-the-system/m-p/1549444#M8541</link>
      <description>&lt;P&gt;Okay, thank you Erich, I got it. Unfortunately our code is too big to fit in RAM only, so that's not an option, we'll just have to deal with it...&lt;/P&gt;&lt;P&gt;Daan&lt;/P&gt;</description>
      <pubDate>Mon, 07 Nov 2022 07:40:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Setting-a-breakpoint-halts-the-system/m-p/1549444#M8541</guid>
      <dc:creator>Daan</dc:creator>
      <dc:date>2022-11-07T07:40:01Z</dc:date>
    </item>
  </channel>
</rss>