<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Cannot end debug session on LPC54016 in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-end-debug-session-on-LPC54016/m-p/1548895#M8538</link>
    <description>&lt;P&gt;Whenever I start a debug session on my LPC54016 board using an LPC-Link 2 interface I can't restart the debug session until I restart MCUXpresso, I simply get the error:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;There is already a running debug session for the launch configuration '[config name removed]'.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I've looked through previous threads and I've used the 'Clean Up Debug' button to no effect. I have no option to terminate the debug session, and Relaunch also fails with the same error. This is highly repeatable and makes debugging practically unusable.&lt;/P&gt;&lt;P&gt;My config options are attached, along with the Console List when this problem is occurring.&lt;/P&gt;&lt;P&gt;Versions:&lt;/P&gt;&lt;P&gt;Ubuntu 22.04.1 LTS&lt;/P&gt;&lt;P&gt;MCUXpresso IDE v11.6.1 [Build 8255] [2022-10-03]&lt;/P&gt;&lt;P&gt;LPC54016 SDK 2.9.0 (435 2021-01-15)&lt;/P&gt;</description>
    <pubDate>Fri, 04 Nov 2022 12:35:27 GMT</pubDate>
    <dc:creator>peter_belm</dc:creator>
    <dc:date>2022-11-04T12:35:27Z</dc:date>
    <item>
      <title>Cannot end debug session on LPC54016</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-end-debug-session-on-LPC54016/m-p/1548895#M8538</link>
      <description>&lt;P&gt;Whenever I start a debug session on my LPC54016 board using an LPC-Link 2 interface I can't restart the debug session until I restart MCUXpresso, I simply get the error:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;There is already a running debug session for the launch configuration '[config name removed]'.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I've looked through previous threads and I've used the 'Clean Up Debug' button to no effect. I have no option to terminate the debug session, and Relaunch also fails with the same error. This is highly repeatable and makes debugging practically unusable.&lt;/P&gt;&lt;P&gt;My config options are attached, along with the Console List when this problem is occurring.&lt;/P&gt;&lt;P&gt;Versions:&lt;/P&gt;&lt;P&gt;Ubuntu 22.04.1 LTS&lt;/P&gt;&lt;P&gt;MCUXpresso IDE v11.6.1 [Build 8255] [2022-10-03]&lt;/P&gt;&lt;P&gt;LPC54016 SDK 2.9.0 (435 2021-01-15)&lt;/P&gt;</description>
      <pubDate>Fri, 04 Nov 2022 12:35:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Cannot-end-debug-session-on-LPC54016/m-p/1548895#M8538</guid>
      <dc:creator>peter_belm</dc:creator>
      <dc:date>2022-11-04T12:35:27Z</dc:date>
    </item>
  </channel>
</rss>