<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Removing heap allocation using linkscripts</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1547626#M8530</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In the project im involved in, we're using nxp product that runs FreeRTOS as os. As our application does not allocate dynamic memory using the ordinary mallocs, I want to remove the heap allocation that the linker puts in the binary.&lt;/P&gt;&lt;P&gt;The method for this is to put the relevant ldt file in the linkscripts folder, which I did- specifically by overriding the heap size to be zero. this works.&lt;/P&gt;&lt;P&gt;How ever, it will be better for me if I could just discard the symbol of the heap from the binary (heap_symbol which is set to _pvHeapStart) because otherwise this symbol gets its address, and it is possible to override memory using its address. My problem is that when im just discarding it I get references errors of gcc files (_cr_sbrk.c) expecting this reference.&lt;/P&gt;&lt;P&gt;I would like to ask for a help reaching my goal which is safely remove the heap allocation from the linker.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 02 Nov 2022 09:06:34 GMT</pubDate>
    <dc:creator>eaad</dc:creator>
    <dc:date>2022-11-02T09:06:34Z</dc:date>
    <item>
      <title>Removing heap allocation using linkscripts</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1547626#M8530</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In the project im involved in, we're using nxp product that runs FreeRTOS as os. As our application does not allocate dynamic memory using the ordinary mallocs, I want to remove the heap allocation that the linker puts in the binary.&lt;/P&gt;&lt;P&gt;The method for this is to put the relevant ldt file in the linkscripts folder, which I did- specifically by overriding the heap size to be zero. this works.&lt;/P&gt;&lt;P&gt;How ever, it will be better for me if I could just discard the symbol of the heap from the binary (heap_symbol which is set to _pvHeapStart) because otherwise this symbol gets its address, and it is possible to override memory using its address. My problem is that when im just discarding it I get references errors of gcc files (_cr_sbrk.c) expecting this reference.&lt;/P&gt;&lt;P&gt;I would like to ask for a help reaching my goal which is safely remove the heap allocation from the linker.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 09:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1547626#M8530</guid>
      <dc:creator>eaad</dc:creator>
      <dc:date>2022-11-02T09:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: Removing heap allocation using linkscripts</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1548151#M8534</link>
      <description>&lt;P&gt;I just want to update that I found a good enough solution, based on this post: &lt;A href="https://stackoverflow.com/questions/40130374/gcc-how-to-disable-heap-usage-entirely-on-an-mcu" target="_blank"&gt;https://stackoverflow.com/questions/40130374/gcc-how-to-disable-heap-usage-entirely-on-an-mcu&lt;/A&gt;&lt;/P&gt;&lt;P&gt;(idea is to redirect dynamic memory allocation methods to unimplemented method, which leads to linker errors if one uses them)&lt;/P&gt;</description>
      <pubDate>Thu, 03 Nov 2022 08:15:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1548151#M8534</guid>
      <dc:creator>eaad</dc:creator>
      <dc:date>2022-11-03T08:15:10Z</dc:date>
    </item>
    <item>
      <title>Re: Removing heap allocation using linkscripts</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1549239#M8540</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/208276"&gt;@eaad&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;In case you want use FreeMarker Scripts or in general check if malloc() is still used, maybe this helps: &lt;A href="https://mcuoneclipse.com/2022/11/06/how-to-make-sure-no-dynamic-memory-is-used/" target="_blank"&gt;https://mcuoneclipse.com/2022/11/06/how-to-make-sure-no-dynamic-memory-is-used/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Sun, 06 Nov 2022 17:27:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1549239#M8540</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2022-11-06T17:27:20Z</dc:date>
    </item>
    <item>
      <title>Re: Removing heap allocation using linkscripts</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1549601#M8543</link>
      <description>&lt;BR /&gt;&lt;BR /&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/17173"&gt;@ErichStyger&lt;/a&gt;, thank you. Actually i was trying the approach of removing the definition of the heap using the FreeMarker Scripts, but I was not able to overcome the __sbrk function error that comes on the linking stage, And even though the map gives me the list, what is a way to overcome that issue?&lt;BR /&gt;&lt;BR /&gt;i get a libc reference:&lt;BR /&gt;&lt;BR /&gt;/usr/local/mcuxpressoide-11.5.1_7266/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.5.1.202201181444/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+dp/hard/libcr_c.a(alloc.o)&lt;BR /&gt;max_utilize_stack.lto_priv.0&lt;BR /&gt;&lt;BR /&gt;what do you think? i couldn't figure that from the article. btw, as you said there, i prefer removing the definition in addition to redirecting the malloc/free ops.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;ty,&lt;BR /&gt;&lt;BR /&gt;Efraim&lt;BR /&gt;</description>
      <pubDate>Mon, 07 Nov 2022 10:23:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1549601#M8543</guid>
      <dc:creator>eaad</dc:creator>
      <dc:date>2022-11-07T10:23:06Z</dc:date>
    </item>
    <item>
      <title>Re: Removing heap allocation using linkscripts</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1549654#M8544</link>
      <description>&lt;P&gt;If __sbrk is still referenced, it means that your application is still possibly calling malloc() or any other dynamic memory allocator.&lt;/P&gt;&lt;P&gt;I suggest you link with the heap in the linker script enabled and then use the Image Info to find out who is calling/using malloc and sbrk. Most likely it is a printf() somewhere in your code?&lt;/P&gt;</description>
      <pubDate>Mon, 07 Nov 2022 11:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1549654#M8544</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2022-11-07T11:47:28Z</dc:date>
    </item>
    <item>
      <title>Re: Removing heap allocation using linkscripts</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1549727#M8546</link>
      <description>&lt;P&gt;Yea, I will re do that, and update about my findings&lt;/P&gt;</description>
      <pubDate>Mon, 07 Nov 2022 14:11:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Removing-heap-allocation-using-linkscripts/m-p/1549727#M8546</guid>
      <dc:creator>eaad</dc:creator>
      <dc:date>2022-11-07T14:11:36Z</dc:date>
    </item>
  </channel>
</rss>