<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Getting an imported Zephyr-project debugged using JLink Interface Debug launch</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Getting-an-imported-Zephyr-project-debugged-using-JLink/m-p/1519473#M8388</link>
    <description>&lt;P&gt;According to NXP's&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/training-reference-material/BUILD-YOUR-FIRST-ZEPHYR-APPLICATION-ON-I.MX-RT.pdf" target="_self"&gt;Build Your First Zephyr Application on i.MX RT&lt;/A&gt;, it is well possible to debug an application that is built using &lt;EM&gt;west build&lt;/EM&gt;. However, the proposed configuration is based on the &lt;U&gt;GDB SEGGER JLINK Interface&lt;/U&gt; Debug, which requires the specification of a SVD-file - which has been found on the local drive but does not populate the peripherals+ view (see&amp;nbsp;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE/How-to-configure-Debug-of-K64F-Zephyr-project-in-Eclipse/m-p/1519296/highlight/true#M8383" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/MCUXpresso-IDE/How-to-configure-Debug-of-K64F-Zephyr-project-in-Eclipse/m-p/1519296/highlight/true#M8383&lt;/A&gt;).&amp;nbsp;&lt;/P&gt;&lt;P&gt;The main objective of &lt;STRONG&gt;this posting&lt;/STRONG&gt; is to get&amp;nbsp;JLink Interface working since this is the default interface for MCUXpresso projects in the case that a &lt;STRONG&gt;Segger firmware&lt;/STRONG&gt; has been activied in the onboard debug hardware. I did flash the Segger firmware a) because the i.MX RT-example supposes its usage and b) because it does not work with the standard DAPlink firmware.&lt;/P&gt;&lt;P&gt;I tried the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Duplicate the debug configuration of a native MCUXpresso example project&lt;/LI&gt;&lt;LI&gt;fill in appropriate paths for e.g. GDB debugger, since a plain&amp;nbsp;&lt;EM&gt;arm-none-eabi-gdb&lt;/EM&gt; does not work, because the imported project is not associated with a &lt;STRONG&gt;C/C++ Build&lt;/STRONG&gt;&amp;nbsp;entry, containing definitions of CWD, PATH and PWD.&lt;/LI&gt;&lt;LI&gt;Debugger Tab Executable path:&amp;nbsp;/usr/bin/JLinkGDBServerCLExe; GDB Client necessarily with full path (&lt;EM&gt;/usr/local/mcuxpressoide-11.5.1_7266/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.5.1.202201181444/tools/bin/arm-none-eabi-gdb&lt;/EM&gt;)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Upon debug session launch I get the following "Problem Occured" window content:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Error in final launch sequence:

Error executing step execute method: stepExecuteExtendedSteps
Error executing step execute method: stepExecuteExtendedSteps
java.lang.reflect.InvocationTargetException&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any hints are appreciated, or even a Kinetis resp. updated version of the i.MX RT pdf...&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Final remark&lt;/STRONG&gt;:The 11.5.0 release document contains a hint regarding the SVD file, but the entry in project properties&amp;nbsp;&lt;SPAN&gt;roject &lt;EM&gt;Properties -&amp;gt; Run/Debug Settings -&amp;gt; MCU Settings&lt;/EM&gt; does not exist, because it was an imported project (according to the pdf).&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 08 Sep 2022 15:13:28 GMT</pubDate>
    <dc:creator>rjm</dc:creator>
    <dc:date>2022-09-08T15:13:28Z</dc:date>
    <item>
      <title>Getting an imported Zephyr-project debugged using JLink Interface Debug launch</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Getting-an-imported-Zephyr-project-debugged-using-JLink/m-p/1519473#M8388</link>
      <description>&lt;P&gt;According to NXP's&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/training-reference-material/BUILD-YOUR-FIRST-ZEPHYR-APPLICATION-ON-I.MX-RT.pdf" target="_self"&gt;Build Your First Zephyr Application on i.MX RT&lt;/A&gt;, it is well possible to debug an application that is built using &lt;EM&gt;west build&lt;/EM&gt;. However, the proposed configuration is based on the &lt;U&gt;GDB SEGGER JLINK Interface&lt;/U&gt; Debug, which requires the specification of a SVD-file - which has been found on the local drive but does not populate the peripherals+ view (see&amp;nbsp;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE/How-to-configure-Debug-of-K64F-Zephyr-project-in-Eclipse/m-p/1519296/highlight/true#M8383" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/MCUXpresso-IDE/How-to-configure-Debug-of-K64F-Zephyr-project-in-Eclipse/m-p/1519296/highlight/true#M8383&lt;/A&gt;).&amp;nbsp;&lt;/P&gt;&lt;P&gt;The main objective of &lt;STRONG&gt;this posting&lt;/STRONG&gt; is to get&amp;nbsp;JLink Interface working since this is the default interface for MCUXpresso projects in the case that a &lt;STRONG&gt;Segger firmware&lt;/STRONG&gt; has been activied in the onboard debug hardware. I did flash the Segger firmware a) because the i.MX RT-example supposes its usage and b) because it does not work with the standard DAPlink firmware.&lt;/P&gt;&lt;P&gt;I tried the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Duplicate the debug configuration of a native MCUXpresso example project&lt;/LI&gt;&lt;LI&gt;fill in appropriate paths for e.g. GDB debugger, since a plain&amp;nbsp;&lt;EM&gt;arm-none-eabi-gdb&lt;/EM&gt; does not work, because the imported project is not associated with a &lt;STRONG&gt;C/C++ Build&lt;/STRONG&gt;&amp;nbsp;entry, containing definitions of CWD, PATH and PWD.&lt;/LI&gt;&lt;LI&gt;Debugger Tab Executable path:&amp;nbsp;/usr/bin/JLinkGDBServerCLExe; GDB Client necessarily with full path (&lt;EM&gt;/usr/local/mcuxpressoide-11.5.1_7266/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.5.1.202201181444/tools/bin/arm-none-eabi-gdb&lt;/EM&gt;)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Upon debug session launch I get the following "Problem Occured" window content:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Error in final launch sequence:

Error executing step execute method: stepExecuteExtendedSteps
Error executing step execute method: stepExecuteExtendedSteps
java.lang.reflect.InvocationTargetException&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any hints are appreciated, or even a Kinetis resp. updated version of the i.MX RT pdf...&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Final remark&lt;/STRONG&gt;:The 11.5.0 release document contains a hint regarding the SVD file, but the entry in project properties&amp;nbsp;&lt;SPAN&gt;roject &lt;EM&gt;Properties -&amp;gt; Run/Debug Settings -&amp;gt; MCU Settings&lt;/EM&gt; does not exist, because it was an imported project (according to the pdf).&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Sep 2022 15:13:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Getting-an-imported-Zephyr-project-debugged-using-JLink/m-p/1519473#M8388</guid>
      <dc:creator>rjm</dc:creator>
      <dc:date>2022-09-08T15:13:28Z</dc:date>
    </item>
    <item>
      <title>Re: Getting an imported Zephyr-project debugged using JLink Interface Debug launch</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Getting-an-imported-Zephyr-project-debugged-using-JLink/m-p/1523183#M8416</link>
      <description>&lt;P&gt;Hi, you need to check the permision and the roules&lt;/P&gt;</description>
      <pubDate>Thu, 15 Sep 2022 21:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Getting-an-imported-Zephyr-project-debugged-using-JLink/m-p/1523183#M8416</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2022-09-15T21:47:12Z</dc:date>
    </item>
  </channel>
</rss>