<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: processor_version: 9.0.3 in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/processor-version-9-0-3/m-p/1519243#M8381</link>
    <description>&lt;P&gt;Testing directly on the project, everything works fine. When opening the pin configuration tool, a warning appears "The loaded configuration was created by an earlier version of the tool. If you save it, you will not be able to reopen the tool with the old version". Then open an IO port at random, update the source code and do nothing else.&lt;BR /&gt;I test again and the error appears, and they are all in resource_config.c&lt;/P&gt;</description>
    <pubDate>Thu, 08 Sep 2022 10:04:08 GMT</pubDate>
    <dc:creator>GaryYJS</dc:creator>
    <dc:date>2022-09-08T10:04:08Z</dc:date>
    <item>
      <title>processor_version: 9.0.3</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/processor-version-9-0-3/m-p/1519048#M8379</link>
      <description>&lt;P&gt;Hello everyone&lt;/P&gt;&lt;P&gt;I have a project where pin_mux.c has the following information.&lt;/P&gt;&lt;P&gt;!!GlobalInfo&lt;BR /&gt;product: Pins v9.0&lt;BR /&gt;processor: LPC55S16&lt;BR /&gt;package_id: LPC55S16JBD100&lt;BR /&gt;mcu_data: ksdk2_0&lt;BR /&gt;processor_version: 9.0.3&lt;BR /&gt;board: LPCXpresso55S16&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where can I download this version of the processor?&lt;/P&gt;&lt;P&gt;When I use the latest version of the IDE and use the pin configuration tool it alerts me that the project version is low. Continuing to use the pin configuration tool to generate the source code causes the project to error out.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Sep 2022 06:43:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/processor-version-9-0-3/m-p/1519048#M8379</guid>
      <dc:creator>GaryYJS</dc:creator>
      <dc:date>2022-09-08T06:43:12Z</dc:date>
    </item>
    <item>
      <title>Re: processor_version: 9.0.3</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/processor-version-9-0-3/m-p/1519163#M8380</link>
      <description>&lt;P&gt;Hello GaryYJS,&lt;/P&gt;
&lt;P&gt;processor 9.0.3 means the MCUX Config Tools v9 were used (MCUXpresso IDE from January 2021). Each version of Config Tools has dedicated set of data that might not be compatible with newer/older version of the tools and it is not expected to be combined this way. Either you should download the older Config Tools or try to fix the issue.&lt;/P&gt;
&lt;P&gt;Can you share what kind of errors do you see? Compile error or during the run-time?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Libor&lt;/P&gt;</description>
      <pubDate>Thu, 08 Sep 2022 08:49:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/processor-version-9-0-3/m-p/1519163#M8380</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2022-09-08T08:49:56Z</dc:date>
    </item>
    <item>
      <title>Re: processor_version: 9.0.3</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/processor-version-9-0-3/m-p/1519243#M8381</link>
      <description>&lt;P&gt;Testing directly on the project, everything works fine. When opening the pin configuration tool, a warning appears "The loaded configuration was created by an earlier version of the tool. If you save it, you will not be able to reopen the tool with the old version". Then open an IO port at random, update the source code and do nothing else.&lt;BR /&gt;I test again and the error appears, and they are all in resource_config.c&lt;/P&gt;</description>
      <pubDate>Thu, 08 Sep 2022 10:04:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/processor-version-9-0-3/m-p/1519243#M8381</guid>
      <dc:creator>GaryYJS</dc:creator>
      <dc:date>2022-09-08T10:04:08Z</dc:date>
    </item>
    <item>
      <title>Re: processor_version: 9.0.3</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/processor-version-9-0-3/m-p/1519581#M8394</link>
      <description>&lt;P&gt;The problem has been solved by using MCUXpressoIDE_11.3.0 which was available on Jan 14, 2021.&lt;/P&gt;&lt;P&gt;Thank you for your help&lt;/P&gt;</description>
      <pubDate>Thu, 08 Sep 2022 20:19:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/processor-version-9-0-3/m-p/1519581#M8394</guid>
      <dc:creator>GaryYJS</dc:creator>
      <dc:date>2022-09-08T20:19:53Z</dc:date>
    </item>
  </channel>
</rss>