<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 LCP4370 Multicore LCPOpen C Project</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/LCP4370-Multicore-LCPOpen-C-Project/m-p/1510385#M8323</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;I am trying to create and build a multicore project for the LCP4370 (LCP-LINK2) Board. However, when I hit build for the master project, I received several error messages saying "No such file or directory" for sys_config.h. sys_config.h is included within chip.h file and chip.h is in the lpc_chip_43xx lib.&lt;BR /&gt;Would appreciate it a lot if you guys can help with this.&lt;/P&gt;</description>
    <pubDate>Tue, 23 Aug 2022 19:37:45 GMT</pubDate>
    <dc:creator>mhpham23</dc:creator>
    <dc:date>2022-08-23T19:37:45Z</dc:date>
    <item>
      <title>LCP4370 Multicore LCPOpen C Project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LCP4370-Multicore-LCPOpen-C-Project/m-p/1510385#M8323</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I am trying to create and build a multicore project for the LCP4370 (LCP-LINK2) Board. However, when I hit build for the master project, I received several error messages saying "No such file or directory" for sys_config.h. sys_config.h is included within chip.h file and chip.h is in the lpc_chip_43xx lib.&lt;BR /&gt;Would appreciate it a lot if you guys can help with this.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Aug 2022 19:37:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LCP4370-Multicore-LCPOpen-C-Project/m-p/1510385#M8323</guid>
      <dc:creator>mhpham23</dc:creator>
      <dc:date>2022-08-23T19:37:45Z</dc:date>
    </item>
    <item>
      <title>Re: LCP4370 Multicore LCPOpen C Project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LCP4370-Multicore-LCPOpen-C-Project/m-p/1512072#M8326</link>
      <description>&lt;P&gt;Hi mhpham23&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please use attached LPC4370 multicore demo code, replacing&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;multicore_mc_sa_blinky demo in lpcopen package&lt;/SPAN&gt;. I ever tested on my side it worked.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Fri, 26 Aug 2022 05:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LCP4370-Multicore-LCPOpen-C-Project/m-p/1512072#M8326</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-08-26T05:02:36Z</dc:date>
    </item>
  </channel>
</rss>