<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: JN5189 connection and board in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/JN5189-connection-and-board/m-p/1504945#M8301</link>
    <description>&lt;P&gt;Hello again. I'd like to explain better:&lt;/P&gt;&lt;P&gt;I have followed the steps from both the PDF you sent me and &lt;A href="https://edit.wpgdadawant.com/uploads/news_file/blog/temp_folder/140_1599634224/tinymce/jn-rn-0064-jn-sw-4470-jn518x-zigbee3-sdk.pdf" target="_self"&gt;this one&lt;/A&gt;,&amp;nbsp; so I got open a main example which I will modify to test my circuits for a simple led blinking. I want my device to use an USB-UART communication for that, which I made following JN518x's Datasheet and &lt;A href="https://www.embedic.com/applications/details/zigbee-relay-routing-scheme-based-on-nxp-jn5189" target="_self"&gt;This article&lt;/A&gt;, So I could say that I want to made a dongle and flash it with the MCUXpresso IDE, without use DK006 board.&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
    <pubDate>Thu, 11 Aug 2022 11:06:01 GMT</pubDate>
    <dc:creator>arivas</dc:creator>
    <dc:date>2022-08-11T11:06:01Z</dc:date>
    <item>
      <title>JN5189 connection and board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/JN5189-connection-and-board/m-p/1503898#M8295</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I've bought several JN5189 MCUs and I've soldered on boards made by myself. They already have an Antenna, capacitors, resistors, oscilator, and everything that official datasheet explains itself.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've also downloaded and installed both MCUXpresso IDE software and jn5189 sdk from the official site.&lt;/P&gt;&lt;P&gt;My objetive: I want to make a simple projects which allows me to communicate at least two devices (one of them as a coordinator and another one as an end device.&lt;/P&gt;&lt;P&gt;So I wanted to try to make my program connecting the device board to my computing using a USB2UART wire, but when I try to start a new project in the IDE, It just let me to select JN5189dk6 board instead of flashing the circuit using its USART ports. How may I make this possible? Any pice of advice?&lt;/P&gt;&lt;P&gt;Thank you and have a nice day!&lt;/P&gt;&lt;P&gt;Adrián Rivas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 10:22:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/JN5189-connection-and-board/m-p/1503898#M8295</guid>
      <dc:creator>arivas</dc:creator>
      <dc:date>2022-08-10T10:22:19Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 connection and board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/JN5189-connection-and-board/m-p/1504364#M8296</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. Just to clarify, do you have a project/example ready to flash? Or are you trying to import and example? Have you tried before with our development kit? (&lt;A target="_blank"&gt;JN5189 Getting Started&lt;/A&gt;) Are you trying to flash the JN5189 via UART? If you have a Development kit, have you tried the Production Flash Programmer?&lt;/P&gt;
&lt;P&gt;Are you planning to use Zigbee or Thread? If you are planning to use ZigBee, please refer to &lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=JN-AN-1260" target="_blank"&gt;Zigbee 3.0 Getting Started&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Thu, 11 Aug 2022 00:46:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/JN5189-connection-and-board/m-p/1504364#M8296</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2022-08-11T00:46:11Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 connection and board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/JN5189-connection-and-board/m-p/1504677#M8299</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for answering. Yes, I 'd like to use one of the examples folliwing the steps on the document below (imported) and I want to flash it into JN5189 via UART0 (PIO8 and 9), but avoiding to use the development kit. I've also read&amp;nbsp;Zigbee 3.0 Getting Started (so useful)&amp;nbsp;but what i need is to connect directly a device to the computer using the UART and your software, but I don't know how can I select that.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Adrian.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Aug 2022 07:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/JN5189-connection-and-board/m-p/1504677#M8299</guid>
      <dc:creator>arivas</dc:creator>
      <dc:date>2022-08-11T07:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 connection and board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/JN5189-connection-and-board/m-p/1504945#M8301</link>
      <description>&lt;P&gt;Hello again. I'd like to explain better:&lt;/P&gt;&lt;P&gt;I have followed the steps from both the PDF you sent me and &lt;A href="https://edit.wpgdadawant.com/uploads/news_file/blog/temp_folder/140_1599634224/tinymce/jn-rn-0064-jn-sw-4470-jn518x-zigbee3-sdk.pdf" target="_self"&gt;this one&lt;/A&gt;,&amp;nbsp; so I got open a main example which I will modify to test my circuits for a simple led blinking. I want my device to use an USB-UART communication for that, which I made following JN518x's Datasheet and &lt;A href="https://www.embedic.com/applications/details/zigbee-relay-routing-scheme-based-on-nxp-jn5189" target="_self"&gt;This article&lt;/A&gt;, So I could say that I want to made a dongle and flash it with the MCUXpresso IDE, without use DK006 board.&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Aug 2022 11:06:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/JN5189-connection-and-board/m-p/1504945#M8301</guid>
      <dc:creator>arivas</dc:creator>
      <dc:date>2022-08-11T11:06:01Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 connection and board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/JN5189-connection-and-board/m-p/1505111#M8303</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The ISP protocol is implemented on USART0 (DIO9 and DIO8). For further information about In-System Programming, please refer to section 38 of the &lt;A href="https://www.nxp.com/webapp/Download?colCode=UM11138" target="_blank"&gt;User Manual&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;The available tool we have for this is the Production Flash Programmer (SDK_JN5189DK6\tools\JN-SW-4407-DK6-Flash-Programmer).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Thu, 11 Aug 2022 16:27:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/JN5189-connection-and-board/m-p/1505111#M8303</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2022-08-11T16:27:35Z</dc:date>
    </item>
  </channel>
</rss>