<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: IEC60730 lib integration problem</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/IEC60730-lib-integration-problem/m-p/1497560#M8259</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203865"&gt;@AlperSefa&lt;/a&gt; which version of MCUXpresso are you using?, Which MCU are using?&lt;/P&gt;</description>
    <pubDate>Thu, 28 Jul 2022 22:33:12 GMT</pubDate>
    <dc:creator>CarlosGarabito</dc:creator>
    <dc:date>2022-07-28T22:33:12Z</dc:date>
    <item>
      <title>IEC60730 lib integration problem</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/IEC60730-lib-integration-problem/m-p/1491567#M8238</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;While adding static lib IEC60730lib , i got some errors about it. Could you help what is the reason of this ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Invoking: MCU Linker&lt;BR /&gt;arm-none-eabi-gcc -nostdlib -L"D:\xxx\safety\v4_1" -L"D:\xxx\safety\v4_1" -Xlinker -Map="xxx.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -Xlinker --sort-section=alignment -Xlinker --cref -mcpu=cortex-m7 -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -T xxx_Debug.ld -L ../linker -o "xxx.axf" ./xip/evkmimxrt1020_flexspi_nor_config.o ./xip/fsl_flexspi_nor_boot.o ./utilities/fsl_debug_console.o ./utilities/fsl_str.o ./startup/startup_mimxrt1021.o ./source/yyy.o ./source/zzz.o ./source/ttt.o ./source/vvv.o ./source/bbb.o ./source/nnn.o ./source/mmm.o ./source/sss.o ./source/ddd.o ./source/fff.o ./source/ggg.o ./source/hhh.o ./source/hhh.o ./source/jjj.o ./source/kkk.o ./source/lll.o ./source/qqq.o ./source/www.o ./source/eee.o ./source/rrr.o ./safety/v4_1/wdog/iec60730b_wdog.o ./safety/safety_cm7_imxrt.o ./safety/safety_test_items.o ./drivers/fsl_clock.o ./drivers/fsl_common.o ./drivers/fsl_common_arm.o ./drivers/fsl_dmamux.o ./drivers/fsl_edma.o ./drivers/fsl_enc.o ./drivers/fsl_flexio.o ./drivers/fsl_flexio_uart.o ./drivers/fsl_gpio.o ./drivers/fsl_lpi2c.o ./drivers/fsl_lpi2c_edma.o ./drivers/fsl_lpuart.o ./drivers/fsl_lpuart_edma.o ./drivers/fsl_pwm.o ./drivers/fsl_qtmr.o ./drivers/fsl_tempmon.o ./drivers/fsl_wdog.o ./drivers/fsl_xbara.o ./device/system_MIMXRT1021.o ./component/uart/fsl_adapter_lpuart.o ./component/serial_manager/fsl_component_serial_manager.o ./component/serial_manager/fsl_component_serial_port_uart.o ./component/lists/fsl_component_generic_list.o ./board/board.o ./board/clock_config.o ./board/dcd.o ./board/peripherals.o ./board/pin_mux.o -lIEC60730B_M4_M7_MCUX_v4_1 -lIEC60730B_M4_M7_COM_MCUX_v4_1&lt;/P&gt;&lt;P&gt;ERROR:&lt;/P&gt;&lt;P&gt;d:/work/nxp/mcuxpressoide_11.5.1_7266/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.5.1.202201181444/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: d:/work/nxp/mcuxpressoide_11.5.1_7266/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.5.1.202201181444/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libcr_semihost_nf.a(_cr__main.o): in function `__main':&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jul 2022 07:36:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/IEC60730-lib-integration-problem/m-p/1491567#M8238</guid>
      <dc:creator>AlperSefa</dc:creator>
      <dc:date>2022-07-19T07:36:22Z</dc:date>
    </item>
    <item>
      <title>Re: IEC60730 lib integration problem</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/IEC60730-lib-integration-problem/m-p/1497560#M8259</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203865"&gt;@AlperSefa&lt;/a&gt; which version of MCUXpresso are you using?, Which MCU are using?&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jul 2022 22:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/IEC60730-lib-integration-problem/m-p/1497560#M8259</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2022-07-28T22:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: IEC60730 lib integration problem</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/IEC60730-lib-integration-problem/m-p/1497990#M8263</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;MCUXpresso IDE v11.5.1 [Build 7266] [2022-04-13]&lt;/P&gt;&lt;P&gt;&amp;nbsp;imxrt1021dag5a&amp;nbsp;&lt;/P&gt;&lt;P&gt;by the way i noticed i can build it in release mode, but i can't compile it in debug mode&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195771" target="_blank"&gt;@CarlosGarabito&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Jul 2022 10:49:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/IEC60730-lib-integration-problem/m-p/1497990#M8263</guid>
      <dc:creator>AlperSefa</dc:creator>
      <dc:date>2022-07-29T10:49:43Z</dc:date>
    </item>
  </channel>
</rss>