<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RT1052 Connection from MCUXpresso with PEMicro Mulitlink Universal FX in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/RT1052-Connection-from-MCUXpresso-with-PEMicro-Mulitlink/m-p/1462628#M8100</link>
    <description>&lt;P&gt;Our board has an RT1052 connected to a QSPI Flash W25Q512JV (so larger than default, and QSPI, not HyperFLASH) part.&lt;/P&gt;&lt;P&gt;What is the expected way to connect MCUXpresso to our board with the PEmicro Multilink Unversal FX?&lt;/P&gt;&lt;P&gt;If I use the LPC-Link2 instead, I can just select the RT1052-QSPI generic loader, and it seems to work fine.&lt;BR /&gt;But if I want to load FLASH via the Multilink FX - seems I need to do a few more things?&lt;/P&gt;&lt;P&gt;See screenshot:&lt;/P&gt;&lt;P&gt;&lt;IMG src="https://user-images.githubusercontent.com/6960865/169879719-3a39dbc1-1e34-49b7-9846-f9ab7991906c.png" border="0" alt="MCUXpresso w PEmicro" width="904" height="1158" /&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 23 May 2022 18:01:25 GMT</pubDate>
    <dc:creator>variable_andrew</dc:creator>
    <dc:date>2022-05-23T18:01:25Z</dc:date>
    <item>
      <title>RT1052 Connection from MCUXpresso with PEMicro Mulitlink Universal FX</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/RT1052-Connection-from-MCUXpresso-with-PEMicro-Mulitlink/m-p/1462628#M8100</link>
      <description>&lt;P&gt;Our board has an RT1052 connected to a QSPI Flash W25Q512JV (so larger than default, and QSPI, not HyperFLASH) part.&lt;/P&gt;&lt;P&gt;What is the expected way to connect MCUXpresso to our board with the PEmicro Multilink Unversal FX?&lt;/P&gt;&lt;P&gt;If I use the LPC-Link2 instead, I can just select the RT1052-QSPI generic loader, and it seems to work fine.&lt;BR /&gt;But if I want to load FLASH via the Multilink FX - seems I need to do a few more things?&lt;/P&gt;&lt;P&gt;See screenshot:&lt;/P&gt;&lt;P&gt;&lt;IMG src="https://user-images.githubusercontent.com/6960865/169879719-3a39dbc1-1e34-49b7-9846-f9ab7991906c.png" border="0" alt="MCUXpresso w PEmicro" width="904" height="1158" /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 23 May 2022 18:01:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/RT1052-Connection-from-MCUXpresso-with-PEMicro-Mulitlink/m-p/1462628#M8100</guid>
      <dc:creator>variable_andrew</dc:creator>
      <dc:date>2022-05-23T18:01:25Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 Connection from MCUXpresso with PEMicro Mulitlink Universal FX</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/RT1052-Connection-from-MCUXpresso-with-PEMicro-Mulitlink/m-p/1462629#M8101</link>
      <description>&lt;P&gt;every time i try to launch with ^^^ - the console only provides the following output:&lt;/P&gt;&lt;P&gt;P&amp;amp;E Semihosting Console&lt;/P&gt;&lt;P&gt;Connection closed by the GDB server.&lt;/P&gt;</description>
      <pubDate>Mon, 23 May 2022 18:08:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/RT1052-Connection-from-MCUXpresso-with-PEMicro-Mulitlink/m-p/1462629#M8101</guid>
      <dc:creator>variable_andrew</dc:creator>
      <dc:date>2022-05-23T18:08:11Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052 Connection from MCUXpresso with PEMicro Mulitlink Universal FX</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/RT1052-Connection-from-MCUXpresso-with-PEMicro-Mulitlink/m-p/1463141#M8103</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/176988"&gt;@variable_andrew&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;No, all there 3 step are not needed. Please keep it as default. But there is one step you must do.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jingpan_0-1653386684249.png" style="width: 696px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/180845iAF487661E9734667/image-dimensions/696x303?v=v2" width="696" height="303" role="button" title="jingpan_0-1653386684249.png" alt="jingpan_0-1653386684249.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 May 2022 10:06:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/RT1052-Connection-from-MCUXpresso-with-PEMicro-Mulitlink/m-p/1463141#M8103</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2022-05-24T10:06:04Z</dc:date>
    </item>
  </channel>
</rss>