<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: LPC54608 UM11035 Dev Board J-Link Debugging</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC54608-UM11035-Dev-Board-J-Link-Debugging/m-p/696897#M803</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It sounds like you are trying to manually set up your launch configuration - this is not what you would normally do using MCUXpresso IDE. Instead you should let the IDE detect your probe, then auto-generate the appropriate launch configuration. The simplest way to do this is to start your debug session using the "Debug" button inside the Quickstart Panel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest looking at the following sections of the MCUXpresso IDE v10.0.2 User Guide for more information...&lt;/P&gt;&lt;P&gt;Chapter 3 - Debug Solutions Overview&lt;/P&gt;&lt;P&gt;Chapter 9 - Debugging a Project&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Oct 2017 14:52:23 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2017-10-03T14:52:23Z</dc:date>
    <item>
      <title>LPC54608 UM11035 Dev Board J-Link Debugging</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC54608-UM11035-Dev-Board-J-Link-Debugging/m-p/696896#M802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the UM11035 Dev board with the LPC54608 MCU. I used LPCScrypt to put the J-Link debugging firmware on the on board debugger. I am able to use&amp;nbsp;JFlashLite.exe to download binaries. But I can't seem to be able to start a debug session through MCUExpresso with the J-Link.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set up GDB Segger Interface Debugging configuration for USB with SWD to use the generated .axf file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I get an error: "Error in final launch sequence Cannot get Jtag device". The debug configuration is set up to do SWD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question:&lt;/P&gt;&lt;P&gt;1) Can this be done?&lt;/P&gt;&lt;P&gt;2) Does the J-Link firmware support semi-hosting?&lt;/P&gt;&lt;P&gt;3) Can I use the dev board with J-Link for the SEGGER SystemView?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Oct 2017 19:04:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPC54608-UM11035-Dev-Board-J-Link-Debugging/m-p/696896#M802</guid>
      <dc:creator>guitardenver</dc:creator>
      <dc:date>2017-10-02T19:04:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 UM11035 Dev Board J-Link Debugging</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC54608-UM11035-Dev-Board-J-Link-Debugging/m-p/696897#M803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It sounds like you are trying to manually set up your launch configuration - this is not what you would normally do using MCUXpresso IDE. Instead you should let the IDE detect your probe, then auto-generate the appropriate launch configuration. The simplest way to do this is to start your debug session using the "Debug" button inside the Quickstart Panel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest looking at the following sections of the MCUXpresso IDE v10.0.2 User Guide for more information...&lt;/P&gt;&lt;P&gt;Chapter 3 - Debug Solutions Overview&lt;/P&gt;&lt;P&gt;Chapter 9 - Debugging a Project&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Oct 2017 14:52:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPC54608-UM11035-Dev-Board-J-Link-Debugging/m-p/696897#M803</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-10-03T14:52:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 UM11035 Dev Board J-Link Debugging</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPC54608-UM11035-Dev-Board-J-Link-Debugging/m-p/696898#M804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Chapter 3 had the answer.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;To answer my other question:&lt;/P&gt;&lt;P&gt;Yes, it on board J-Link can be used to debug.&lt;/P&gt;&lt;P&gt;Yes, the J-Link does support semihosting.&lt;/P&gt;&lt;P&gt;Yes, it can be used with SystemView&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Oct 2017 16:51:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPC54608-UM11035-Dev-Board-J-Link-Debugging/m-p/696898#M804</guid>
      <dc:creator>guitardenver</dc:creator>
      <dc:date>2017-10-03T16:51:11Z</dc:date>
    </item>
  </channel>
</rss>