<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: LPCXpresso54S018M SDRAM initialization script for debugging?</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1421768#M7874</link>
    <description>&lt;P&gt;No, we don't have such a script.&lt;/P&gt;
&lt;P&gt;The boot ROM&amp;nbsp; facilitates loading images into on-chip SRAM and provides from external memory (internal serial flash, Nor Flash, spi norflash, etc). this is done in boot rom already.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For more, see LPC54S018M UM.&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
    <pubDate>Wed, 02 Mar 2022 09:14:40 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2022-03-02T09:14:40Z</dc:date>
    <item>
      <title>LPCXpresso54S018M SDRAM initialization script for debugging?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1420059#M7860</link>
      <description>&lt;P&gt;I need to be able to debug code running in SDRAM.&amp;nbsp; I built and linked the code for SDRAM, but the debug configuration needs to initialize the SDRAM before loading the code into it.&amp;nbsp; I looked in the MCUXpresso &amp;lt;install dir&amp;gt;/ide/binaries/Scripts but can't find a script to use to initialize the SDRAM on the board so I can debug in SDRAM?&amp;nbsp; Is there a script available that someone could point me to?&lt;/P&gt;</description>
      <pubDate>Sun, 27 Feb 2022 00:03:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1420059#M7860</guid>
      <dc:creator>john_c_kennedy</dc:creator>
      <dc:date>2022-02-27T00:03:29Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso54S018M SDRAM initialization script for debugging?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1421083#M7865</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please refer this AN "SDRAM Code Execution in LPC5460x". It's also for LPC54018&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12423.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12423.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Tue, 01 Mar 2022 08:43:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1421083#M7865</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-03-01T08:43:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso54S018M SDRAM initialization script for debugging?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1421325#M7868</link>
      <description>&lt;P&gt;Thanks but AN12423 doesn't have an SDRAM initialization script for debugging in SDRAM using the MCUXpresso IDE.&amp;nbsp; Surley this is a common request from developers using either the LPC54S018M-EVK or the LPC54S018-EVK boards?&amp;nbsp; It's hard to beleive that NXP doesn't have an SDRAM initialization script for debugging software from SDRAM on these boards since they were made for development?&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;</description>
      <pubDate>Tue, 01 Mar 2022 16:45:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1421325#M7868</guid>
      <dc:creator>john_c_kennedy</dc:creator>
      <dc:date>2022-03-01T16:45:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso54S018M SDRAM initialization script for debugging?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1421768#M7874</link>
      <description>&lt;P&gt;No, we don't have such a script.&lt;/P&gt;
&lt;P&gt;The boot ROM&amp;nbsp; facilitates loading images into on-chip SRAM and provides from external memory (internal serial flash, Nor Flash, spi norflash, etc). this is done in boot rom already.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For more, see LPC54S018M UM.&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Wed, 02 Mar 2022 09:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1421768#M7874</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-03-02T09:14:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso54S018M SDRAM initialization script for debugging?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1423510#M7893</link>
      <description>&lt;P&gt;See this:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Blogs/Overview-of-using-the-MIMXRT1050-EVK-B-with-MCUXpresso-IDE/ba-p/1131013" target="_blank"&gt;https://community.nxp.com/t5/Blogs/Overview-of-using-the-MIMXRT1050-EVK-B-with-MCUXpresso-IDE/ba-p/1131013&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This is the same thing I would like to do except with the LPC54S018-EVK or LPC54S018M-EVK.&amp;nbsp; It seems if this is possible with the MIMXRT1050-EVK it should be possible with the LPC54S018(M)-EVK?&lt;/P&gt;</description>
      <pubDate>Sat, 05 Mar 2022 17:15:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1423510#M7893</guid>
      <dc:creator>john_c_kennedy</dc:creator>
      <dc:date>2022-03-05T17:15:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso54S018M SDRAM initialization script for debugging?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1423787#M7901</link>
      <description>&lt;P&gt;NO. we don't have same script for &lt;SPAN&gt;LPC54S018(M)-EVK&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Mar 2022 08:53:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/LPCXpresso54S018M-SDRAM-initialization-script-for-debugging/m-p/1423787#M7901</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-03-07T08:53:29Z</dc:date>
    </item>
  </channel>
</rss>