<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Set PROGRAM_FLASH value in the IDE settings in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Set-PROGRAM-FLASH-value-in-the-IDE-settings/m-p/1386412#M7670</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/17173"&gt;@ErichStyger&lt;/a&gt;&amp;nbsp; ,&lt;/P&gt;&lt;P&gt;Thank you very much for the reply and help.&lt;/P&gt;&lt;P&gt;I am glad to hear that you have already&amp;nbsp;&lt;SPAN&gt;filed a feature request on this , so I look forward to see it implemented on the next versions of the MCUxpresso, as it would help a lot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you also for the link on a way to work around this issue. I will try to implement it for sure.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 14 Dec 2021 11:30:49 GMT</pubDate>
    <dc:creator>joao_ribeiro</dc:creator>
    <dc:date>2021-12-14T11:30:49Z</dc:date>
    <item>
      <title>Set PROGRAM_FLASH value in the IDE settings</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Set-PROGRAM-FLASH-value-in-the-IDE-settings/m-p/1385792#M7666</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have a project where we would like to have the opportunity to compile it for using a bootloader version and compile it for a version without bootloader. For that I am using the compile in debug mode or in release mode, changing the code accordingly with #if DEBUG and #endif . But to totally accomplish it, we would like to change the&amp;nbsp;PROGRAM_FLASH as well , setting it to 0xf000 for the bootloader and 0 for the debug version .&lt;/P&gt;&lt;P&gt;I am trying to find a way to do so but the MCUxpresso Properties-&amp;gt;MCU settings are not defined by the compile mode, therefore I always have to change the&amp;nbsp;PROGRAM_FLASH address every time I want to change the mode.&lt;/P&gt;&lt;P&gt;Is there a way to link the address to the compile mode so that the transition is just linked with the compilation mode?&lt;/P&gt;&lt;P&gt;Thank you for the help&lt;/P&gt;&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 17:21:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Set-PROGRAM-FLASH-value-in-the-IDE-settings/m-p/1385792#M7666</guid>
      <dc:creator>joao_ribeiro</dc:creator>
      <dc:date>2021-12-13T17:21:58Z</dc:date>
    </item>
    <item>
      <title>Re: Set PROGRAM_FLASH value in the IDE settings</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Set-PROGRAM-FLASH-value-in-the-IDE-settings/m-p/1386148#M7667</link>
      <description>&lt;P&gt;See my article on this topic at &lt;A href="https://mcuoneclipse.com/2019/10/06/linking-bootloader-applications-with-eclipse-and-freemarker-scripts/" target="_blank"&gt;https://mcuoneclipse.com/2019/10/06/linking-bootloader-applications-with-eclipse-and-freemarker-scripts/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;As you noted, the memory map/MCU settings do not support build configurations. I have filed a feature request on this, so I hope this could be available in a future version. Until then, the above approach with freemarker scripts works very well for me: I can build the booloader app or the standalone app. As long as the device stays the same with its overall memory map. Which is usually the case.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 07:21:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Set-PROGRAM-FLASH-value-in-the-IDE-settings/m-p/1386148#M7667</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2021-12-14T07:21:49Z</dc:date>
    </item>
    <item>
      <title>Re: Set PROGRAM_FLASH value in the IDE settings</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Set-PROGRAM-FLASH-value-in-the-IDE-settings/m-p/1386412#M7670</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/17173"&gt;@ErichStyger&lt;/a&gt;&amp;nbsp; ,&lt;/P&gt;&lt;P&gt;Thank you very much for the reply and help.&lt;/P&gt;&lt;P&gt;I am glad to hear that you have already&amp;nbsp;&lt;SPAN&gt;filed a feature request on this , so I look forward to see it implemented on the next versions of the MCUxpresso, as it would help a lot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you also for the link on a way to work around this issue. I will try to implement it for sure.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 11:30:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Set-PROGRAM-FLASH-value-in-the-IDE-settings/m-p/1386412#M7670</guid>
      <dc:creator>joao_ribeiro</dc:creator>
      <dc:date>2021-12-14T11:30:49Z</dc:date>
    </item>
  </channel>
</rss>