<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PNEV7462C - Failed to execute MI command in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/PNEV7462C-Failed-to-execute-MI-command/m-p/1384100#M7652</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to program the PNEV7462C demokit with the example NfcrdlibEx4_MIFAREClassic_mcux example. It compiles fine (I had to change the target MCU for the right one) but when it comes to uploading it, either by debug or to flash, I get the following error:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Error in final launch sequence:&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Failed to execute MI command:&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;-target-select extended-remote | crt_emu_cm_redlink -msg-port=62459 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP --connectscript=ISPResetConnect.scp --resetscript=ISPResetConnect.scp --reset= -ProbeHandle=1 -CoreIndex=0 --flash-hashing --flash-driver FTFA_4K.cfx -x C:/Users/Julien/Documents/MCUXpressoIDE_11.4.1_6260/workspace/NxpNfcRdLib_PN7462_v06.10.00_Pub/Examples/NfcrdlibEx4_MIFAREClassic/mcux/DebugPN7462AU --telnet 3330&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Error message from debugger back end:&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Remote communication error. Target disconnected.: No error.&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Failed to execute MI command:&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;-target-select extended-remote | crt_emu_cm_redlink -msg-port=62459 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP --connectscript=ISPResetConnect.scp --resetscript=ISPResetConnect.scp --reset= -ProbeHandle=1 -CoreIndex=0 --flash-hashing --flash-driver FTFA_4K.cfx -x C:/Users/Julien/Documents/MCUXpressoIDE_11.4.1_6260/workspace/NxpNfcRdLib_PN7462_v06.10.00_Pub/Examples/NfcrdlibEx4_MIFAREClassic/mcux/DebugPN7462AU --telnet 3330&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Error message from debugger back end:&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;This error is strange since I can program without issue many other example such as the PN7462AU_ex_phExVcom_mcux.&lt;/P&gt;&lt;P&gt;Is there a step I'm missing?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 09 Dec 2021 15:31:10 GMT</pubDate>
    <dc:creator>JM0</dc:creator>
    <dc:date>2021-12-09T15:31:10Z</dc:date>
    <item>
      <title>PNEV7462C - Failed to execute MI command</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/PNEV7462C-Failed-to-execute-MI-command/m-p/1384100#M7652</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to program the PNEV7462C demokit with the example NfcrdlibEx4_MIFAREClassic_mcux example. It compiles fine (I had to change the target MCU for the right one) but when it comes to uploading it, either by debug or to flash, I get the following error:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Error in final launch sequence:&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Failed to execute MI command:&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;-target-select extended-remote | crt_emu_cm_redlink -msg-port=62459 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP --connectscript=ISPResetConnect.scp --resetscript=ISPResetConnect.scp --reset= -ProbeHandle=1 -CoreIndex=0 --flash-hashing --flash-driver FTFA_4K.cfx -x C:/Users/Julien/Documents/MCUXpressoIDE_11.4.1_6260/workspace/NxpNfcRdLib_PN7462_v06.10.00_Pub/Examples/NfcrdlibEx4_MIFAREClassic/mcux/DebugPN7462AU --telnet 3330&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Error message from debugger back end:&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Remote communication error. Target disconnected.: No error.&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Failed to execute MI command:&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;-target-select extended-remote | crt_emu_cm_redlink -msg-port=62459 -g -mi -2 -pPN7462AU-C3-00 -vendor=NXP --connectscript=ISPResetConnect.scp --resetscript=ISPResetConnect.scp --reset= -ProbeHandle=1 -CoreIndex=0 --flash-hashing --flash-driver FTFA_4K.cfx -x C:/Users/Julien/Documents/MCUXpressoIDE_11.4.1_6260/workspace/NxpNfcRdLib_PN7462_v06.10.00_Pub/Examples/NfcrdlibEx4_MIFAREClassic/mcux/DebugPN7462AU --telnet 3330&lt;/EM&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#999999"&gt;&lt;EM&gt;Error message from debugger back end:&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;This error is strange since I can program without issue many other example such as the PN7462AU_ex_phExVcom_mcux.&lt;/P&gt;&lt;P&gt;Is there a step I'm missing?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 09 Dec 2021 15:31:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/PNEV7462C-Failed-to-execute-MI-command/m-p/1384100#M7652</guid>
      <dc:creator>JM0</dc:creator>
      <dc:date>2021-12-09T15:31:10Z</dc:date>
    </item>
    <item>
      <title>Re: PNEV7462C - Failed to execute MI command</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/PNEV7462C-Failed-to-execute-MI-command/m-p/1390184#M7683</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/193878"&gt;@JM0&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I would suggest you try to&amp;nbsp; perform a mass erase with MCUXpresso in case this issue happens.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielchen_0-1640092938507.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/165843iECCF37EDA467E3E8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielchen_0-1640092938507.png" alt="danielchen_0-1640092938507.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Dec 2021 13:23:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/PNEV7462C-Failed-to-execute-MI-command/m-p/1390184#M7683</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2021-12-21T13:23:16Z</dc:date>
    </item>
  </channel>
</rss>