<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: Individual commands ISO15693</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Individual-commands-ISO15693/m-p/1355569#M7542</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192331"&gt;@mark2030&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The API of "phpalSli15693_Exchange" can be used for that purpose. Please kindly refer to&amp;nbsp;phpalSli15693.c for more details.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 14 Oct 2021 06:15:08 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2021-10-14T06:15:08Z</dc:date>
    <item>
      <title>Individual commands ISO15693</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Individual-commands-ISO15693/m-p/1354301#M7533</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I work with the CLRC663 chip and read IO15693 transponders.&lt;/P&gt;&lt;P&gt;When I call the function phalI15693_ReadMultipleBlocks () everything works as described.&lt;/P&gt;&lt;P&gt;The bytes: SOF 20 23 [UID] FBN NOB CRC CRC EOF are sent via RFID.&lt;/P&gt;&lt;P&gt;But now I need an individual command in the following form:&lt;BR /&gt;SOF 20 AB 02 [UID]&lt;/P&gt;&lt;P&gt;AB is the command and 02 is a constant. How can I configure such individual commands?&lt;/P&gt;&lt;P&gt;Many thanks for your help&lt;/P&gt;</description>
      <pubDate>Tue, 12 Oct 2021 14:30:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Individual-commands-ISO15693/m-p/1354301#M7533</guid>
      <dc:creator>mark2030</dc:creator>
      <dc:date>2021-10-12T14:30:00Z</dc:date>
    </item>
    <item>
      <title>Re: Individual commands ISO15693</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Individual-commands-ISO15693/m-p/1355569#M7542</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192331"&gt;@mark2030&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The API of "phpalSli15693_Exchange" can be used for that purpose. Please kindly refer to&amp;nbsp;phpalSli15693.c for more details.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 14 Oct 2021 06:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Individual-commands-ISO15693/m-p/1355569#M7542</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-10-14T06:15:08Z</dc:date>
    </item>
  </channel>
</rss>