<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 not able to debug with j-link</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/not-able-to-debug-with-j-link/m-p/1344974#M7448</link>
    <description>&lt;P&gt;I have the following problem.&lt;/P&gt;&lt;P&gt;With the latest version of mcuxpresso and the LPC55s16-EVK and the onboard debug-probe everything works fine. With an own pcb with the LPC55S16JBD64 and an J-Link EDU with the latest drivers, it compiles, seems to transfer the image on the MCU. But i have no resume button. only suspend, terminate and restart. sometimes on start of debugsession, ResetISR() from startup_lpc55s16.c gets opened an in the debug view is shown: Thread #1 57005(Running: User Request) and arm-none-eabi-gdb (10.1.90.20201028)&lt;/P&gt;&lt;P&gt;what i'm doing wrong, that debugging does not work?&lt;/P&gt;&lt;P&gt;the J-Link Web Control shows that target is connected&lt;/P&gt;</description>
    <pubDate>Thu, 23 Sep 2021 09:29:53 GMT</pubDate>
    <dc:creator>RRD101</dc:creator>
    <dc:date>2021-09-23T09:29:53Z</dc:date>
    <item>
      <title>not able to debug with j-link</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/not-able-to-debug-with-j-link/m-p/1344974#M7448</link>
      <description>&lt;P&gt;I have the following problem.&lt;/P&gt;&lt;P&gt;With the latest version of mcuxpresso and the LPC55s16-EVK and the onboard debug-probe everything works fine. With an own pcb with the LPC55S16JBD64 and an J-Link EDU with the latest drivers, it compiles, seems to transfer the image on the MCU. But i have no resume button. only suspend, terminate and restart. sometimes on start of debugsession, ResetISR() from startup_lpc55s16.c gets opened an in the debug view is shown: Thread #1 57005(Running: User Request) and arm-none-eabi-gdb (10.1.90.20201028)&lt;/P&gt;&lt;P&gt;what i'm doing wrong, that debugging does not work?&lt;/P&gt;&lt;P&gt;the J-Link Web Control shows that target is connected&lt;/P&gt;</description>
      <pubDate>Thu, 23 Sep 2021 09:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/not-able-to-debug-with-j-link/m-p/1344974#M7448</guid>
      <dc:creator>RRD101</dc:creator>
      <dc:date>2021-09-23T09:29:53Z</dc:date>
    </item>
    <item>
      <title>Re: not able to debug with j-link</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/not-able-to-debug-with-j-link/m-p/1377628#M7625</link>
      <description>&lt;P&gt;problem solved. PIO0_5 was in the wrong state&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Nov 2021 12:09:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/not-able-to-debug-with-j-link/m-p/1377628#M7625</guid>
      <dc:creator>RRD101</dc:creator>
      <dc:date>2021-11-26T12:09:38Z</dc:date>
    </item>
  </channel>
</rss>