<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: Can I use a script with MCUXpresso LinkServer debug sessions?</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Can-I-use-a-script-with-MCUXpresso-LinkServer-debug-sessions/m-p/1326863#M7313</link>
    <description>&lt;P&gt;Thank you TIC!&lt;/P&gt;&lt;P&gt;I have had a look at the User Guide but I don't think it provides much help for working with gdb.&lt;/P&gt;&lt;P&gt;In the end I believe this is simply that 'run' is not a valid command to use in a gdb script (i.e. .gdbinit).&lt;/P&gt;&lt;P&gt;'run' is achieved by unchecking 'Debug configurations -&amp;gt; Startup -&amp;gt; Run Commands -&amp;gt; Set breakpoint at:'&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
    <pubDate>Fri, 20 Aug 2021 09:47:11 GMT</pubDate>
    <dc:creator>robert_s</dc:creator>
    <dc:date>2021-08-20T09:47:11Z</dc:date>
    <item>
      <title>Can I use a script with MCUXpresso LinkServer debug sessions?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Can-I-use-a-script-with-MCUXpresso-LinkServer-debug-sessions/m-p/1322714#M7283</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Firstly I'm new to MCUXpresso!...&lt;/P&gt;&lt;P&gt;I have built one of the demo SDK examples for the 'i.MX RT 1170' (&lt;A href="https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-rt1170-evaluation-kit:MIMXRT1170-EVK?tid=vaniMXRT1170EVK)" target="_blank"&gt;https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-rt1170-evaluation-kit:MIMXRT1170-EVK?tid=vaniMXRT1170EVK)&lt;/A&gt; and am able start and debug via a LinkServer Debug Configuration.&lt;/P&gt;&lt;P&gt;By default, the debugger stops at the first executable statement in main().&lt;/P&gt;&lt;P&gt;I would then like the debug session to execute a 'script', such as a .gdb file.&lt;/P&gt;&lt;P&gt;I tried creating a file for the 'GDB command file' under the 'GDB Debugger' tab of my Debug Configuration, but always fails with:&lt;/P&gt;&lt;P&gt;&amp;lt;edited&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Error in final launch sequence:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Failed to execute MI command:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; source .gdb&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Error message from debugger back end:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .gdb:2: Error in sourced command file:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The program is not being run.&lt;/P&gt;&lt;P&gt;So the .gdb file does get used, even for a LinkServer seesion&lt;/P&gt;&lt;P&gt;Thank you for help you can provide.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Aug 2021 15:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Can-I-use-a-script-with-MCUXpresso-LinkServer-debug-sessions/m-p/1322714#M7283</guid>
      <dc:creator>robert_s</dc:creator>
      <dc:date>2021-08-12T15:23:55Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use a script with MCUXpresso LinkServer debug sessions?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Can-I-use-a-script-with-MCUXpresso-LinkServer-debug-sessions/m-p/1324435#M7307</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;To provide the fastest possible support, I'd recommend you try to refer to the &lt;A href="https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf" target="_self"&gt;MCUXpresso IDE User Guide&lt;/A&gt;.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 07:07:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Can-I-use-a-script-with-MCUXpresso-LinkServer-debug-sessions/m-p/1324435#M7307</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-08-17T07:07:21Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use a script with MCUXpresso LinkServer debug sessions?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Can-I-use-a-script-with-MCUXpresso-LinkServer-debug-sessions/m-p/1326863#M7313</link>
      <description>&lt;P&gt;Thank you TIC!&lt;/P&gt;&lt;P&gt;I have had a look at the User Guide but I don't think it provides much help for working with gdb.&lt;/P&gt;&lt;P&gt;In the end I believe this is simply that 'run' is not a valid command to use in a gdb script (i.e. .gdbinit).&lt;/P&gt;&lt;P&gt;'run' is achieved by unchecking 'Debug configurations -&amp;gt; Startup -&amp;gt; Run Commands -&amp;gt; Set breakpoint at:'&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Fri, 20 Aug 2021 09:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Can-I-use-a-script-with-MCUXpresso-LinkServer-debug-sessions/m-p/1326863#M7313</guid>
      <dc:creator>robert_s</dc:creator>
      <dc:date>2021-08-20T09:47:11Z</dc:date>
    </item>
    <item>
      <title>Re: Can I use a script with MCUXpresso LinkServer debug sessions?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Can-I-use-a-script-with-MCUXpresso-LinkServer-debug-sessions/m-p/1327577#M7317</link>
      <description>&lt;P&gt;For a remote target, 'run' is not an appropriate command. The command you want is 'continue'.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Aug 2021 08:11:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Can-I-use-a-script-with-MCUXpresso-LinkServer-debug-sessions/m-p/1327577#M7317</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-08-23T08:11:15Z</dc:date>
    </item>
  </channel>
</rss>