<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Linker script search paths</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Linker-script-search-paths/m-p/1325525#M7310</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In the MCUXpresso IDE User Manual, section 17.14.2 (Linkerscript) Reference, the manual states "&lt;EM&gt;The searchPath can be set in a script by using the syntax &amp;lt;#global searchPath=“c:/windows/path;d:/another/windows/path”&amp;gt;&lt;/EM&gt;".&lt;/P&gt;&lt;P&gt;Is there an example on what this script is to look like and how to implement it?&lt;/P&gt;</description>
    <pubDate>Wed, 18 Aug 2021 14:57:28 GMT</pubDate>
    <dc:creator>chadgraham</dc:creator>
    <dc:date>2021-08-18T14:57:28Z</dc:date>
    <item>
      <title>Linker script search paths</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Linker-script-search-paths/m-p/1325525#M7310</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In the MCUXpresso IDE User Manual, section 17.14.2 (Linkerscript) Reference, the manual states "&lt;EM&gt;The searchPath can be set in a script by using the syntax &amp;lt;#global searchPath=“c:/windows/path;d:/another/windows/path”&amp;gt;&lt;/EM&gt;".&lt;/P&gt;&lt;P&gt;Is there an example on what this script is to look like and how to implement it?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 14:57:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Linker-script-search-paths/m-p/1325525#M7310</guid>
      <dc:creator>chadgraham</dc:creator>
      <dc:date>2021-08-18T14:57:28Z</dc:date>
    </item>
    <item>
      <title>Re: Linker script search paths</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Linker-script-search-paths/m-p/1326390#M7312</link>
      <description>&lt;P&gt;The listing of search paths in section 17.14.2 can be tricky, but it demonstrates the order in which MCUXpresso searches for the scripts to create the linker files. It first looks inside the scripts under &lt;EM&gt;project/linkscripts&lt;/EM&gt;, and then searches on the path specified by the &lt;EM&gt;searchPath&lt;/EM&gt; global variable. As the User Manual states, this variable should be set “in a script”. Therefore, you would have to make a new one and place it under &lt;EM&gt;project/linkscripts&lt;/EM&gt; to set a new definition of searchPath. This way, after looking under &lt;EM&gt;project/linkscripts&lt;/EM&gt;, there will be a definition of this variable and MCUXpresso will be able to look for the specified paths. Since it was written by the user, this script should be the “user.ldt” file. This one has the highest priority on the hierarchy because it contains the user variables that will be used in the rest of the scripts.&lt;/P&gt;
&lt;P&gt;Erich Styger demonstrates the creation of new FreeMarker scripts on this post; Perhaps you will find it useful: &lt;A href="https://mcuoneclipse.com/2019/10/06/linking-bootloader-applications-with-eclipse-and-freemarker-scripts/" target="_blank"&gt;https://mcuoneclipse.com/2019/10/06/linking-bootloader-applications-with-eclipse-and-freemarker-scripts/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this helps,&lt;/P&gt;
&lt;P&gt;Edwin.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Aug 2021 18:00:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Linker-script-search-paths/m-p/1326390#M7312</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2021-08-19T18:00:14Z</dc:date>
    </item>
  </channel>
</rss>