<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: Interrupt frequency determination</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Interrupt-frequency-determination/m-p/1275921#M6952</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Hope you are well. I will gladly help you with this.&lt;BR /&gt;You can determine the frequency of a signal with the FTM module. You can find an example of it at AN5142 under chapter 3.8 &lt;A href="https://www.nxp.com/docs/en/application-note/AN5142.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5142.pdf&lt;/A&gt;&lt;BR /&gt;You can add a timer into the interruption handler to determine the period but I suggest using the FTM method to determine the frequency of a signal.&lt;/P&gt;
&lt;P&gt;The PendSV is commonly used in RTOS applications and is used for context switch, the interruption is given by the SysTick.&lt;BR /&gt;&lt;BR /&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Wed, 12 May 2021 21:26:42 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2021-05-12T21:26:42Z</dc:date>
    <item>
      <title>Interrupt frequency determination</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Interrupt-frequency-determination/m-p/1273488#M6941</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I wanted to know how:&lt;/P&gt;&lt;P&gt;1. I will be able to set a GPIO interrupt lets say PORTE and determine at what frequency it runs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. How to determine at what frequency an interrupt from the compare module runs? Where should I be giving the interrupt timing interval?&lt;/P&gt;&lt;P&gt;3. PendSV interrupt frequency determination?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 07 May 2021 07:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Interrupt-frequency-determination/m-p/1273488#M6941</guid>
      <dc:creator>soaring_sun</dc:creator>
      <dc:date>2021-05-07T07:38:24Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt frequency determination</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Interrupt-frequency-determination/m-p/1275921#M6952</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Hope you are well. I will gladly help you with this.&lt;BR /&gt;You can determine the frequency of a signal with the FTM module. You can find an example of it at AN5142 under chapter 3.8 &lt;A href="https://www.nxp.com/docs/en/application-note/AN5142.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5142.pdf&lt;/A&gt;&lt;BR /&gt;You can add a timer into the interruption handler to determine the period but I suggest using the FTM method to determine the frequency of a signal.&lt;/P&gt;
&lt;P&gt;The PendSV is commonly used in RTOS applications and is used for context switch, the interruption is given by the SysTick.&lt;BR /&gt;&lt;BR /&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 12 May 2021 21:26:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Interrupt-frequency-determination/m-p/1275921#M6952</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-05-12T21:26:42Z</dc:date>
    </item>
  </channel>
</rss>