<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: Add binary file to a project</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Add-binary-file-to-a-project/m-p/1241911#M6779</link>
    <description>&lt;P&gt;Does this help?&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE/Binary-File-as-resource-for-project/m-p/606014" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE/Binary-File-as-resource-for-project/m-p/606014&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 08 Mar 2021 18:01:00 GMT</pubDate>
    <dc:creator>converse</dc:creator>
    <dc:date>2021-03-08T18:01:00Z</dc:date>
    <item>
      <title>Add binary file to a project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Add-binary-file-to-a-project/m-p/1241660#M6776</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would add to my project the binary file of the bootloader. In this way during board production, the operator can program the device only one time. Is there any way to do this?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;</description>
      <pubDate>Mon, 08 Mar 2021 09:34:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Add-binary-file-to-a-project/m-p/1241660#M6776</guid>
      <dc:creator>MarcoGiammarini</dc:creator>
      <dc:date>2021-03-08T09:34:37Z</dc:date>
    </item>
    <item>
      <title>Re: Add binary file to a project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Add-binary-file-to-a-project/m-p/1241674#M6777</link>
      <description>&lt;P&gt;I think you need to provide more information on what you are trying to do. What is the binary file? What are you expecting a bootloader to do with it?&lt;/P&gt;</description>
      <pubDate>Mon, 08 Mar 2021 10:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Add-binary-file-to-a-project/m-p/1241674#M6777</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-03-08T10:02:12Z</dc:date>
    </item>
    <item>
      <title>Re: Add binary file to a project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Add-binary-file-to-a-project/m-p/1241675#M6778</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144226"&gt;@converse&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;thanks for your replay. Into my application, I want to add the binary image of the bootloader (It is a different project) at a specific address. In this way, I can generate during compilation only one file that includes the bootloader and application. At this time, the operator that program the board, do this operation only one time and not one time for bootloader and one time for application.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marco&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Mar 2021 10:08:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Add-binary-file-to-a-project/m-p/1241675#M6778</guid>
      <dc:creator>MarcoGiammarini</dc:creator>
      <dc:date>2021-03-08T10:08:55Z</dc:date>
    </item>
    <item>
      <title>Re: Add binary file to a project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Add-binary-file-to-a-project/m-p/1241911#M6779</link>
      <description>&lt;P&gt;Does this help?&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE/Binary-File-as-resource-for-project/m-p/606014" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE/Binary-File-as-resource-for-project/m-p/606014&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Mar 2021 18:01:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Add-binary-file-to-a-project/m-p/1241911#M6779</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-03-08T18:01:00Z</dc:date>
    </item>
  </channel>
</rss>