<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: ADC module operation</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1236781#M6742</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183199"&gt;@soaring_sun&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You're understanding is right. The CLIST defines the channel sample according to the user needs and in case you need to sample multiple times has the advantage that, depending on the mode enabled in the ADC_CTRL1.SMODE, you can perform sequential or parallel conversions.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
    <pubDate>Thu, 25 Feb 2021 17:56:31 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2021-02-25T17:56:31Z</dc:date>
    <item>
      <title>ADC module operation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1229743#M6701</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I wanted to use an ADC for measurements. In the previous microcontrollers that I had been using, I used to connect the PWM pin to the ADC, which starts calculating the values at compare match. Once the calculations are done, the ADC triggers an interrupt where the next actions take place.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But after going through the reference manual and related posts, I understand that an FTM is used to trigger the ADC, correct? Or will I be able to follow the same procedure as stated above? Or does ADC work independently without having to use any trigger mechanism?&lt;/P&gt;&lt;P&gt;There is no example that explains the ADC module usage. Help me out.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Feb 2021 08:30:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1229743#M6701</guid>
      <dc:creator>soaring_sun</dc:creator>
      <dc:date>2021-02-11T08:30:34Z</dc:date>
    </item>
    <item>
      <title>Re: ADC module operation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1230191#M6705</link>
      <description>&lt;P&gt;Okay, so I found that inspite of triggering the ADC with various other methods (using FTM, DMA...) it can also be triggered using PWM pin. The reference manual states so in both the ADC and PWM sub headings. The following is the reference manual that I'm referring.&lt;/P&gt;&lt;P&gt;&lt;A title="TRM" href="https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true" target="_self"&gt;mkv46f256vll16_reference_manual&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.PNG" style="width: 823px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137088iF1DC0D8E166751F9/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.PNG" style="width: 599px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137089i66727D49107E85DD/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But no where in the manual it is said how to access these bits. Or is it something I'm missing. I have also gone through a few inbuilt functions. But I don't see any that comes close to this. Although, I found one information regarding the same under &lt;STRONG&gt;PWMA_DTSRCSEL&lt;/STRONG&gt; heading, but it states that it is mainly used for the dead-time calculations. So, if I'm not using a dead time for that particular PWM, operating it in the independent mode, then is this bit acting as a external trigger to ADC?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.PNG" style="width: 814px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137091iDE44A3C9C84754AA/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If so, then I should be using the inbuilt function&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Capture.PNG" style="width: 455px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137092i3AF3A2070B686BB3/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But it is just not making any sense to me. Please help me out with this, asap.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Feb 2021 06:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1230191#M6705</guid>
      <dc:creator>soaring_sun</dc:creator>
      <dc:date>2021-02-12T06:14:57Z</dc:date>
    </item>
    <item>
      <title>Re: ADC module operation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1233776#M6724</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183199"&gt;@soaring_sun&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;In the &lt;A href="https://mcuxpresso.nxp.com/" target="_self"&gt;SDK&lt;/A&gt;, in the section of demo examples, there's one called cadc_pwm_trigger, the registers are accessed using the&amp;nbsp; XBARA_SetSignalsConnection API.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Fri, 19 Feb 2021 17:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1233776#M6724</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-02-19T17:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: ADC module operation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1234082#M6728</link>
      <description>&lt;P&gt;Yes! I found them, thank you.&lt;/P&gt;&lt;P&gt;So, to conclude there are two ADCs - ADCA and ADCB both having 0 to 7 channels with a total of 15 ADC channels for analog calculations. The result of them can be configured to the CLIST 1 to 4 according to the user needs.&lt;/P&gt;&lt;P&gt;Here, in the in built function,&lt;/P&gt;&lt;P&gt;void CADC_SetSampleConfig(ADC_Type *base, uint16_t sampleIndex, const cadc_sample_config_t *config);&lt;/P&gt;&lt;P&gt;the sample index can vary from 0 to 15 and the same number cannot be used to measure more than one ADC value.&lt;/P&gt;&lt;P&gt;Am I right about this?&lt;/P&gt;&lt;P&gt;Help me understand better. Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 22 Feb 2021 03:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1234082#M6728</guid>
      <dc:creator>soaring_sun</dc:creator>
      <dc:date>2021-02-22T03:56:57Z</dc:date>
    </item>
    <item>
      <title>Re: ADC module operation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1236781#M6742</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/183199"&gt;@soaring_sun&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You're understanding is right. The CLIST defines the channel sample according to the user needs and in case you need to sample multiple times has the advantage that, depending on the mode enabled in the ADC_CTRL1.SMODE, you can perform sequential or parallel conversions.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Thu, 25 Feb 2021 17:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1236781#M6742</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-02-25T17:56:31Z</dc:date>
    </item>
    <item>
      <title>Re: ADC module operation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1237020#M6743</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/167559"&gt;@Alexis_A&lt;/a&gt;&amp;nbsp;That clears my doubts.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Feb 2021 05:16:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/ADC-module-operation/m-p/1237020#M6743</guid>
      <dc:creator>soaring_sun</dc:creator>
      <dc:date>2021-02-26T05:16:24Z</dc:date>
    </item>
  </channel>
</rss>