<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCUXpresso No data was programmed in FLASH in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-No-data-was-programmed-in-FLASH/m-p/1224183#M6654</link>
    <description>&lt;P&gt;Hi Pietro,&lt;/P&gt;&lt;P&gt;if you created the project for the wrong processor type, it is much easier and simpler if you create a new project for the correct processor than tweaking an existing one. You would have to change project defines, project settings up to changing settings in project files referencing the SDK.&lt;/P&gt;&lt;P&gt;Create a new fresh project and copy your own source files over.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 01 Feb 2021 16:54:35 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2021-02-01T16:54:35Z</dc:date>
    <item>
      <title>MCUXpresso No data was programmed in FLASH</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-No-data-was-programmed-in-FLASH/m-p/1223767#M6649</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am trying to program the TWR-K20D72M board with the JTAG, using the flasj tool in MCUXpresso.&lt;/P&gt;&lt;P&gt;I load the elf file and that's the message on the console&lt;/P&gt;&lt;P&gt;Executing flash operation 'Program' (Program file into flash: uV1.4.elf) - Mon Feb 01 06:45:36 CET 2021&lt;BR /&gt;Checking MCU info...&lt;BR /&gt;Scanning for targets...&lt;BR /&gt;Executing flash action...&lt;BR /&gt;P&amp;amp;E GDB Server for Arm(R) devices, Version 8.35.00.00&lt;BR /&gt;Copyright 2018, P&amp;amp;E Microcomputer Systems Inc, All rights reserved&lt;BR /&gt;Loading library C:\MXP\MCUXpressoIDE_11.3.0_5222\ide\plugins\com.pemicro.debug.gdbjtag.pne_4.8.5.202101062027\win32\gdi\unit_ngs_arm_internal.dll ... Done.&lt;BR /&gt;Command line arguments: -interface=USBMULTILINK -port=USB1 -speed=5000 -flashobjectfile=C:\PietroWorks\ClimbRobot\FromJonas\uTaskerV1.4.elf -device=NXP_K2x_K20DX256M10 -programmingtype=0 -runafterprogramming -startserver -singlesession -quitafterprogramming&lt;BR /&gt;Device selected is NXP_K2x_K20DX256M10&lt;BR /&gt;User Specified Hardware Selection : Interface=USBMULTILINK and Port=USB1&lt;BR /&gt;Connecting to target.&lt;BR /&gt;P&amp;amp;E Interface detected - Flash Version 6.15&lt;BR /&gt;Soft reset failed!&lt;BR /&gt;Device is Secure.&lt;BR /&gt;Device is secured. Erasing ...&lt;BR /&gt;Device is NXP_K2x_K20DX256M10.&lt;BR /&gt;Mode is In-Circuit Debug.&lt;BR /&gt;(C)opyright 2012, P&amp;amp;E Microcomputer Systems, Inc. (&lt;A href="http://www.pemicro.com" target="_blank"&gt;www.pemicro.com&lt;/A&gt;)&lt;BR /&gt;API version is 101&lt;BR /&gt;TARGET XML PATH is C:\MXP\MCUXpressoIDE_11.3.0_5222\ide\plugins\com.pemicro.debug.gdbjtag.pne_4.8.5.202101062027\win32\gdi\P&amp;amp;E\supportFiles_ARM\target_v7m_no_vfp.xml&lt;BR /&gt;USING FREERTOS CORTEX-M V6 (NO FPU) DRIVERS&lt;BR /&gt;Server 1 running on 127.0.0.1:7224&lt;BR /&gt;Server 2 running on 127.0.0.1:7226&lt;BR /&gt;Server 3 running on 127.0.0.1:7228&lt;BR /&gt;Server 4 running on 127.0.0.1:7230&lt;BR /&gt;Server 5 running on 127.0.0.1:7232&lt;BR /&gt;Server 6 running on 127.0.0.1:7234&lt;BR /&gt;Server 7 running on 127.0.0.1:7236&lt;BR /&gt;Server 8 running on 127.0.0.1:7238&lt;BR /&gt;Server 9 running on 127.0.0.1:7240&lt;BR /&gt;Server 10 running on 127.0.0.1:7242&lt;BR /&gt;Warning: No data was programmed in FLASH&lt;BR /&gt;All Servers Running&lt;BR /&gt;Target Disconnected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What's there??&lt;/P&gt;&lt;P&gt;Thank You for help&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 05:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-No-data-was-programmed-in-FLASH/m-p/1223767#M6649</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2021-02-01T05:56:13Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso No data was programmed in FLASH</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-No-data-was-programmed-in-FLASH/m-p/1223770#M6650</link>
      <description>&lt;P&gt;Just asking and checking if the hardware/connection works fine otherwise.&lt;/P&gt;&lt;P&gt;are you able to debug that board using the normal 'blue' debug button?&lt;/P&gt;&lt;P&gt;or does this fail too?&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 05:59:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-No-data-was-programmed-in-FLASH/m-p/1223770#M6650</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2021-02-01T05:59:11Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso No data was programmed in FLASH</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-No-data-was-programmed-in-FLASH/m-p/1224080#M6652</link>
      <description>&lt;P&gt;Hei Erich&lt;/P&gt;&lt;P&gt;It seems I need to change manually the processor type to the VLL7 on the board.&amp;nbsp;&lt;BR /&gt;I tried to launch the blue button is another disaster.&lt;/P&gt;&lt;P&gt;For now I would like to focus on the programming... The file I am using is working on another machine I cannot access now. So I need at least to reply the result here.&lt;/P&gt;&lt;P&gt;Suggest me how to change manually the processor type to the VLL/&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 12:41:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-No-data-was-programmed-in-FLASH/m-p/1224080#M6652</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2021-02-01T12:41:03Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso No data was programmed in FLASH</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-No-data-was-programmed-in-FLASH/m-p/1224179#M6653</link>
      <description>&lt;P&gt;Hi Erich&lt;/P&gt;&lt;P&gt;I am giving up for the moment.&lt;/P&gt;&lt;P&gt;I will need a fresh mind. Now I am tired to analize this. Whatever it is it needs to be simple.&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 16:47:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-No-data-was-programmed-in-FLASH/m-p/1224179#M6653</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2021-02-01T16:47:41Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso No data was programmed in FLASH</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-No-data-was-programmed-in-FLASH/m-p/1224183#M6654</link>
      <description>&lt;P&gt;Hi Pietro,&lt;/P&gt;&lt;P&gt;if you created the project for the wrong processor type, it is much easier and simpler if you create a new project for the correct processor than tweaking an existing one. You would have to change project defines, project settings up to changing settings in project files referencing the SDK.&lt;/P&gt;&lt;P&gt;Create a new fresh project and copy your own source files over.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 16:54:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-No-data-was-programmed-in-FLASH/m-p/1224183#M6654</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2021-02-01T16:54:35Z</dc:date>
    </item>
  </channel>
</rss>