<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: Program flash from command line without IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Program-flash-from-command-line-without-IDE/m-p/1221420#M6607</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/77802"&gt;@nickwallis&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;see as well&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2020/12/05/standalone-and-command-line-programmer-with-mcuxpresso/" target="_blank"&gt;https://mcuoneclipse.com/2020/12/05/standalone-and-command-line-programmer-with-mcuxpresso/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
    <pubDate>Tue, 26 Jan 2021 19:14:25 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2021-01-26T19:14:25Z</dc:date>
    <item>
      <title>Program flash from command line without IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Program-flash-from-command-line-without-IDE/m-p/1221337#M6599</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;Is it possible to program flash from a command line without either (1) installing the IDE at all or (2) with the IDE installed, but without invoking the IDE?&lt;/P&gt;&lt;P&gt;This is for JTAG/SWD programming using an external programmer like a J-LINK, not something that communicates with the bootloader using USB or UART.&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jan 2021 15:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Program-flash-from-command-line-without-IDE/m-p/1221337#M6599</guid>
      <dc:creator>nickwallis</dc:creator>
      <dc:date>2021-01-26T15:55:08Z</dc:date>
    </item>
    <item>
      <title>Re: Program flash from command line without IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Program-flash-from-command-line-without-IDE/m-p/1221349#M6601</link>
      <description>&lt;P&gt;Yes. Read the User manual - the section on the GUI flash tool describes how you can use the tool from the command line. You do need the whole product installed though.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;depending on your target, you may also be able to use Flash Magic. Also Segger have a stand-alone tool, but I think you have to purchase it for commercial use.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jan 2021 16:12:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Program-flash-from-command-line-without-IDE/m-p/1221349#M6601</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-01-26T16:12:35Z</dc:date>
    </item>
    <item>
      <title>Re: Program flash from command line without IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Program-flash-from-command-line-without-IDE/m-p/1221420#M6607</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/77802"&gt;@nickwallis&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;see as well&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2020/12/05/standalone-and-command-line-programmer-with-mcuxpresso/" target="_blank"&gt;https://mcuoneclipse.com/2020/12/05/standalone-and-command-line-programmer-with-mcuxpresso/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jan 2021 19:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Program-flash-from-command-line-without-IDE/m-p/1221420#M6607</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2021-01-26T19:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: Program flash from command line without IDE</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Program-flash-from-command-line-without-IDE/m-p/1222063#M6621</link>
      <description>&lt;P&gt;Thanks &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144226"&gt;@converse&lt;/a&gt;&amp;nbsp; &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/17173"&gt;@ErichStyger&lt;/a&gt;&amp;nbsp;, this seems to work OK for me from the command line but I do see the following error (?) message at the end, does it matter?&lt;/P&gt;&lt;P&gt;regards Nick&lt;/P&gt;&lt;P&gt;..........&lt;/P&gt;&lt;P&gt;Nc: Sectors written: 4, unchanged: 0, total: 4&lt;BR /&gt;Nc: Closing flash driver MIMXRT1060_SFDP_QSPI.cfx&lt;BR /&gt;Nt: Loaded 0x330F0 bytes in 4028ms (about 51kB/s)&lt;BR /&gt;Nt: Reset target (system)&lt;BR /&gt;Nc: Starting execution using system reset&lt;BR /&gt;Nc: state - running or following reset request - re-read of state failed - rc Nn(05). &lt;U&gt;&lt;STRONG&gt;Wire ACK Fault&lt;/STRONG&gt;&lt;/U&gt; in DAP access&lt;BR /&gt;Xw:&lt;BR /&gt;Nc: error closing down debug session - Nn(05). &lt;U&gt;&lt;STRONG&gt;Wire ACK Fault in DAP access&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jan 2021 17:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Program-flash-from-command-line-without-IDE/m-p/1222063#M6621</guid>
      <dc:creator>nickwallis</dc:creator>
      <dc:date>2021-01-27T17:19:15Z</dc:date>
    </item>
  </channel>
</rss>