<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックFreeRTOS stack backtrace is disabled</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/FreeRTOS-stack-backtrace-is-disabled/m-p/1193218#M6440</link>
    <description>&lt;P&gt;I am testing FreeRTOS on an LPCXpresso board:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Board: LPCXpresso LPC1769 (rev. C)&lt;/LI&gt;&lt;LI&gt;IDE: MCUXpresso 11.2.1 [Build 4149] (2020-10-07)&lt;/LI&gt;&lt;LI&gt;Library: LPCOpen v2.10 [2014-12-03]&lt;/LI&gt;&lt;LI&gt;Operating system: FreeRTOS 10.4.1&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I have followed the prompts for "MCUXpresso IDE FreeRTOS Debug Guide" (Rev. 11.2.0 - 7 October, 2020) from NXP:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I have copied the header file "freertos_tasks_c_additions.h" from &amp;lt;install dir&amp;gt; / ide / Examples / Misc to the same folder as "FreeRTOSConfig.h".&lt;/LI&gt;&lt;LI&gt;The file "tasks.c" already comes with the code that includes the file "freertos_tasks_c_additions.h", so it is not necessary to modify it.&lt;/LI&gt;&lt;LI&gt;I have defined the following macros in FreeRTOSConfig.h:&lt;UL&gt;&lt;LI&gt;#define configINCLUDE_FREERTOS_TASK_C_ADDITIONS_H 1&lt;/LI&gt;&lt;LI&gt;#define configUSE_TRACE_FACILITY 1&lt;/LI&gt;&lt;LI&gt;#define configRECORD_STACK_HIGH_ADDRESS 1&lt;/LI&gt;&lt;LI&gt;#define configGENERATE_RUN_TIME_STATS 1 (and I have also defined the macros portCONFIGURE_TIMER_FOR_RUN_TIME_STATS () and portGET_RUN_TIME_COUNTER_VALUE ())&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;And in the file "freertos_tasks_c_additions.h":&lt;UL&gt;&lt;LI&gt;#define configFRTOS_MEMORY_SCHEME 1 (I'm using heap_1.c)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;However, the FreeRTOS TAD task list appears empty and only the current task is displayed in the debug view.&lt;/P&gt;&lt;P&gt;I have been able to fix the task list thanks to &lt;A href="https://mcuoneclipse.com/2017/03/18/better-freertos-debugging-in-eclipse/" target="_blank" rel="noopener"&gt;https://mcuoneclipse.com/2017/03/18/better-freertos-debugging-in-eclipse/&lt;/A&gt;&amp;nbsp; By disabling the legacy API names in FreeRTOSConfig.h (#define configENABLE_BACKWARD_COMPATIBILITY 0) the task list fills up as if by magic. (I don't know if it is a very specific case, but it would be nice if it was indicated in the FreeRTOS Debug Guide; It would have saved me many hours of frustration).&lt;/P&gt;&lt;P&gt;But despite the fact that the project compiles, runs and works fine, despite the fact that the three tasks (plus the idle) that compose it are displayed in the FreeRTOS TAD task list (with their execution times), in the debug view only shows the current task, the one that was running when stopped.&lt;/P&gt;&lt;P&gt;I copy below the content of the debugging console, because I think the key may be there:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;MCUXpresso IDE RedlinkMulti Driver v11.2 (Sep 22 2020 13:23:35 - crt_emu_cm_redlink build 19)
Found part description in XML file nxp_lpc17xx.xme
Reconnected to existing LinkServer process.
Probe Firmware: LPC-Link Probe v1.3 (NXP - LPC-Link)
Serial Number: WIN64HS12
VID: PID: 1FC9: 0009
USB Path:
Using memory from core 0 after searching for a good core
debug interface type = Cortex-M3 / 4 (DAP DP ID 2BA01477) over SWD TAP 0
processor type = Cortex-M3 (CPU ID 00000C23) on DAP AP 0
number of h / w breakpoints = 6
number of flash patches = 2
number of h / w watchpoints = 4
Probe (0): Connected &amp;amp; Reset. DpID: 2BA01477. CpuID: 00000C23. Info: &amp;lt;None&amp;gt;
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Content of CoreSight Debug ROM (s):
RBASE E00FF000: CID B105100D PID 0000000000 ROM (type 0x1)
ROM 1 E000E000: CID B105E00D PID 04002BB000 Gen SCS (type 0x0)
ROM 1 E0001000: CID B105E00D PID 04002BB002 Gen DWT (type 0x0)
ROM 1 E0002000: CID B105E00D PID 04002BB003 Gen FPB (type 0x0)
ROM 1 E0000000: CID B105E00D PID 04002BB001 Gen ITM (type 0x0)
ROM 1 E0040000: CID B105900D PID 04002BB923 CSt TPIU-Lite type 0x11 Trace Sink - TPIU
ROM 1 E0041000: CID B105900D PID 04002BB924 CSt ETM-M3 type 0x13 Trace Source - Core
NXP: LPC1769
DAP stride is 4096 bytes (1024 words)
Inspected v.2 On-chip Flash Memory LPC175x_6x_512.cfx
Image 'LPC175x_6x (512K) Sep 25 2020 10:47:33'
Connected: was_reset = true. was_stopped = false
Awaiting telnet connection to port 3336 ...
GDB nonstop mode disabled (using allstop mode)
Opening flash driver LPC175x_6x_512.cfx
Sending VECTRESET to run flash driver
Flash device supported (512KB = 16 * 4K 14 * 32K at 0x0)
Writing 7340 bytes to address 0x00000000 in Flash
Sectors written: 0, unchanged: 2, total: 2
Erased / Wrote sector 0-1 with 7340 bytes in 38msec
Closing flash driver LPC175x_6x_512.cfx
Flash Write Done
Flash Program Summary: 7340 bytes in 0.04 seconds (188.63 KB / sec)
Starting execution using core reset and halt target
Stopped (Was Reset) [Reset from Unknown]
Stopped: Breakpoint # 1
Stopped: Halt&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As you can see I am debugging in All-Stop mode. However, I don't get the message "FreeRTOS stack backtrace is enabled". Following the instructions of the FreeRTOS Debug Guide I have added a folder called "linkscripts" to the root directory of the project and I have created a file "user.ldt" with the content:&lt;BR /&gt;&amp;lt;#assign force_freertos = true&amp;gt;&lt;/P&gt;&lt;P&gt;It seems that something has improved, as it now mentions FreeRTOS, but it is not the expected result:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;GDB nonstop mode disabled (using allstop mode)
FreeRTOS stack backtrace is disabled&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why? Can somebody help me? I insist that the project compiles, runs and works correctly. Tasks are displayed in FreeRTOS TAD task list, execution times are consistent. I can successfully debug the project ... The only problem is that the debug view only shows the current task.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="freertosBacktraceDisable.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/131538i9D4057741E092F6D/image-size/large?v=v2&amp;amp;px=999" role="button" title="freertosBacktraceDisable.png" alt="freertosBacktraceDisable.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;freertosBacktraceDisable.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;</description>
    <pubDate>Thu, 03 Dec 2020 12:40:48 GMT</pubDate>
    <dc:creator>asiertapiazulai</dc:creator>
    <dc:date>2020-12-03T12:40:48Z</dc:date>
    <item>
      <title>FreeRTOS stack backtrace is disabled</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/FreeRTOS-stack-backtrace-is-disabled/m-p/1193218#M6440</link>
      <description>&lt;P&gt;I am testing FreeRTOS on an LPCXpresso board:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Board: LPCXpresso LPC1769 (rev. C)&lt;/LI&gt;&lt;LI&gt;IDE: MCUXpresso 11.2.1 [Build 4149] (2020-10-07)&lt;/LI&gt;&lt;LI&gt;Library: LPCOpen v2.10 [2014-12-03]&lt;/LI&gt;&lt;LI&gt;Operating system: FreeRTOS 10.4.1&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I have followed the prompts for "MCUXpresso IDE FreeRTOS Debug Guide" (Rev. 11.2.0 - 7 October, 2020) from NXP:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I have copied the header file "freertos_tasks_c_additions.h" from &amp;lt;install dir&amp;gt; / ide / Examples / Misc to the same folder as "FreeRTOSConfig.h".&lt;/LI&gt;&lt;LI&gt;The file "tasks.c" already comes with the code that includes the file "freertos_tasks_c_additions.h", so it is not necessary to modify it.&lt;/LI&gt;&lt;LI&gt;I have defined the following macros in FreeRTOSConfig.h:&lt;UL&gt;&lt;LI&gt;#define configINCLUDE_FREERTOS_TASK_C_ADDITIONS_H 1&lt;/LI&gt;&lt;LI&gt;#define configUSE_TRACE_FACILITY 1&lt;/LI&gt;&lt;LI&gt;#define configRECORD_STACK_HIGH_ADDRESS 1&lt;/LI&gt;&lt;LI&gt;#define configGENERATE_RUN_TIME_STATS 1 (and I have also defined the macros portCONFIGURE_TIMER_FOR_RUN_TIME_STATS () and portGET_RUN_TIME_COUNTER_VALUE ())&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;And in the file "freertos_tasks_c_additions.h":&lt;UL&gt;&lt;LI&gt;#define configFRTOS_MEMORY_SCHEME 1 (I'm using heap_1.c)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;However, the FreeRTOS TAD task list appears empty and only the current task is displayed in the debug view.&lt;/P&gt;&lt;P&gt;I have been able to fix the task list thanks to &lt;A href="https://mcuoneclipse.com/2017/03/18/better-freertos-debugging-in-eclipse/" target="_blank" rel="noopener"&gt;https://mcuoneclipse.com/2017/03/18/better-freertos-debugging-in-eclipse/&lt;/A&gt;&amp;nbsp; By disabling the legacy API names in FreeRTOSConfig.h (#define configENABLE_BACKWARD_COMPATIBILITY 0) the task list fills up as if by magic. (I don't know if it is a very specific case, but it would be nice if it was indicated in the FreeRTOS Debug Guide; It would have saved me many hours of frustration).&lt;/P&gt;&lt;P&gt;But despite the fact that the project compiles, runs and works fine, despite the fact that the three tasks (plus the idle) that compose it are displayed in the FreeRTOS TAD task list (with their execution times), in the debug view only shows the current task, the one that was running when stopped.&lt;/P&gt;&lt;P&gt;I copy below the content of the debugging console, because I think the key may be there:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;MCUXpresso IDE RedlinkMulti Driver v11.2 (Sep 22 2020 13:23:35 - crt_emu_cm_redlink build 19)
Found part description in XML file nxp_lpc17xx.xme
Reconnected to existing LinkServer process.
Probe Firmware: LPC-Link Probe v1.3 (NXP - LPC-Link)
Serial Number: WIN64HS12
VID: PID: 1FC9: 0009
USB Path:
Using memory from core 0 after searching for a good core
debug interface type = Cortex-M3 / 4 (DAP DP ID 2BA01477) over SWD TAP 0
processor type = Cortex-M3 (CPU ID 00000C23) on DAP AP 0
number of h / w breakpoints = 6
number of flash patches = 2
number of h / w watchpoints = 4
Probe (0): Connected &amp;amp; Reset. DpID: 2BA01477. CpuID: 00000C23. Info: &amp;lt;None&amp;gt;
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Content of CoreSight Debug ROM (s):
RBASE E00FF000: CID B105100D PID 0000000000 ROM (type 0x1)
ROM 1 E000E000: CID B105E00D PID 04002BB000 Gen SCS (type 0x0)
ROM 1 E0001000: CID B105E00D PID 04002BB002 Gen DWT (type 0x0)
ROM 1 E0002000: CID B105E00D PID 04002BB003 Gen FPB (type 0x0)
ROM 1 E0000000: CID B105E00D PID 04002BB001 Gen ITM (type 0x0)
ROM 1 E0040000: CID B105900D PID 04002BB923 CSt TPIU-Lite type 0x11 Trace Sink - TPIU
ROM 1 E0041000: CID B105900D PID 04002BB924 CSt ETM-M3 type 0x13 Trace Source - Core
NXP: LPC1769
DAP stride is 4096 bytes (1024 words)
Inspected v.2 On-chip Flash Memory LPC175x_6x_512.cfx
Image 'LPC175x_6x (512K) Sep 25 2020 10:47:33'
Connected: was_reset = true. was_stopped = false
Awaiting telnet connection to port 3336 ...
GDB nonstop mode disabled (using allstop mode)
Opening flash driver LPC175x_6x_512.cfx
Sending VECTRESET to run flash driver
Flash device supported (512KB = 16 * 4K 14 * 32K at 0x0)
Writing 7340 bytes to address 0x00000000 in Flash
Sectors written: 0, unchanged: 2, total: 2
Erased / Wrote sector 0-1 with 7340 bytes in 38msec
Closing flash driver LPC175x_6x_512.cfx
Flash Write Done
Flash Program Summary: 7340 bytes in 0.04 seconds (188.63 KB / sec)
Starting execution using core reset and halt target
Stopped (Was Reset) [Reset from Unknown]
Stopped: Breakpoint # 1
Stopped: Halt&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As you can see I am debugging in All-Stop mode. However, I don't get the message "FreeRTOS stack backtrace is enabled". Following the instructions of the FreeRTOS Debug Guide I have added a folder called "linkscripts" to the root directory of the project and I have created a file "user.ldt" with the content:&lt;BR /&gt;&amp;lt;#assign force_freertos = true&amp;gt;&lt;/P&gt;&lt;P&gt;It seems that something has improved, as it now mentions FreeRTOS, but it is not the expected result:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;GDB nonstop mode disabled (using allstop mode)
FreeRTOS stack backtrace is disabled&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why? Can somebody help me? I insist that the project compiles, runs and works correctly. Tasks are displayed in FreeRTOS TAD task list, execution times are consistent. I can successfully debug the project ... The only problem is that the debug view only shows the current task.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="freertosBacktraceDisable.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/131538i9D4057741E092F6D/image-size/large?v=v2&amp;amp;px=999" role="button" title="freertosBacktraceDisable.png" alt="freertosBacktraceDisable.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;freertosBacktraceDisable.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 12:40:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/FreeRTOS-stack-backtrace-is-disabled/m-p/1193218#M6440</guid>
      <dc:creator>asiertapiazulai</dc:creator>
      <dc:date>2020-12-03T12:40:48Z</dc:date>
    </item>
  </channel>
</rss>