<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: Failed to create System Restore Point</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Failed-to-create-System-Restore-Point/m-p/1188608#M6410</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/154346"&gt;@xgy_upc&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I would say this is more of a problem of Windows than MCUXpresso. I had this a while back when I did not have enough disk space available for Windows (less than 1 GByte free). Not sure if this is the case for you. Other than that, the installation should go fine.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
    <pubDate>Wed, 25 Nov 2020 05:23:08 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2020-11-25T05:23:08Z</dc:date>
    <item>
      <title>Failed to create System Restore Point</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Failed-to-create-System-Restore-Point/m-p/1188559#M6409</link>
      <description>&lt;P&gt;&lt;SPAN&gt;When installing MCUXpresso IDE on a 64-bit Win10 System, the prompt "Failed to create System Restore Point "appears&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 03:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Failed-to-create-System-Restore-Point/m-p/1188559#M6409</guid>
      <dc:creator>xgy_upc</dc:creator>
      <dc:date>2020-11-25T03:30:26Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to create System Restore Point</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Failed-to-create-System-Restore-Point/m-p/1188608#M6410</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/154346"&gt;@xgy_upc&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I would say this is more of a problem of Windows than MCUXpresso. I had this a while back when I did not have enough disk space available for Windows (less than 1 GByte free). Not sure if this is the case for you. Other than that, the installation should go fine.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 05:23:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Failed-to-create-System-Restore-Point/m-p/1188608#M6410</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2020-11-25T05:23:08Z</dc:date>
    </item>
  </channel>
</rss>