<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: Launching with reset without flashing</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/Launching-with-reset-without-flashing/m-p/1176183#M6306</link>
    <description>&lt;P&gt;That might depend on the debug probe you are using: for example you have more scripting with J-Link than with other probes, and the scripting is depending on the probe.&lt;/P&gt;&lt;P&gt;You could use a modified 'run' configuration (see&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2014/10/04/emulating-eclipse-run-with-debug-configuration/" target="_blank"&gt;https://mcuoneclipse.com/2014/10/04/emulating-eclipse-run-with-debug-configuration/&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;So basically you could do a 'connect' followed by a 'reset' and 'disconnect'. You could look into GDB commands too (&lt;A href="https://mcuoneclipse.com/2015/03/25/command-line-programming-and-debugging-with-gdb/" target="_blank"&gt;https://mcuoneclipse.com/2015/03/25/command-line-programming-and-debugging-with-gdb/&lt;/A&gt; ).&amp;nbsp;&lt;/P&gt;&lt;P&gt;The LinkServer Connection has some settings too, but not sure if you could call a script there:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ErichS_0-1604144211749.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128755i77555DA20B2EC604/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ErichS_0-1604144211749.png" alt="ErichS_0-1604144211749.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
    <pubDate>Sat, 31 Oct 2020 11:37:13 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2020-10-31T11:37:13Z</dc:date>
    <item>
      <title>Launching with reset without flashing</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Launching-with-reset-without-flashing/m-p/1176125#M6294</link>
      <description>&lt;P&gt;Is there a way to setup a launch profile that resets the mcu without flashing a new image?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not talking about just attaching, I want a full reset but I want to keep the same code on the device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Possible?&lt;/P&gt;</description>
      <pubDate>Sat, 31 Oct 2020 00:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Launching-with-reset-without-flashing/m-p/1176125#M6294</guid>
      <dc:creator>alannilsson</dc:creator>
      <dc:date>2020-10-31T00:07:04Z</dc:date>
    </item>
    <item>
      <title>Re: Launching with reset without flashing</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/Launching-with-reset-without-flashing/m-p/1176183#M6306</link>
      <description>&lt;P&gt;That might depend on the debug probe you are using: for example you have more scripting with J-Link than with other probes, and the scripting is depending on the probe.&lt;/P&gt;&lt;P&gt;You could use a modified 'run' configuration (see&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2014/10/04/emulating-eclipse-run-with-debug-configuration/" target="_blank"&gt;https://mcuoneclipse.com/2014/10/04/emulating-eclipse-run-with-debug-configuration/&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;So basically you could do a 'connect' followed by a 'reset' and 'disconnect'. You could look into GDB commands too (&lt;A href="https://mcuoneclipse.com/2015/03/25/command-line-programming-and-debugging-with-gdb/" target="_blank"&gt;https://mcuoneclipse.com/2015/03/25/command-line-programming-and-debugging-with-gdb/&lt;/A&gt; ).&amp;nbsp;&lt;/P&gt;&lt;P&gt;The LinkServer Connection has some settings too, but not sure if you could call a script there:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ErichS_0-1604144211749.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128755i77555DA20B2EC604/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ErichS_0-1604144211749.png" alt="ErichS_0-1604144211749.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Sat, 31 Oct 2020 11:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/Launching-with-reset-without-flashing/m-p/1176183#M6306</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2020-10-31T11:37:13Z</dc:date>
    </item>
  </channel>
</rss>