<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDE中的主题 Re: FreeRTOS thread aware debugging on static RTOS</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/FreeRTOS-thread-aware-debugging-on-static-RTOS/m-p/1175465#M6288</link>
    <description>&lt;P&gt;The 'All-Stop' setting when setting up the launch config does not stick. &amp;nbsp;Delete all launch configs, create a new one and select 'All-Stop' -&amp;gt; does not work. &amp;nbsp;Stop debugging and open launch config properties and 'non-stop' is check marked. &amp;nbsp;Uncheck that and debug then it works.&lt;/P&gt;&lt;P&gt;This happens on both versions 10.2 &amp;amp; 11.1&lt;/P&gt;&lt;P&gt;In the end it is now working for me, case closed.&lt;/P&gt;</description>
    <pubDate>Thu, 29 Oct 2020 18:34:03 GMT</pubDate>
    <dc:creator>alannilsson</dc:creator>
    <dc:date>2020-10-29T18:34:03Z</dc:date>
    <item>
      <title>FreeRTOS thread aware debugging on static RTOS</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/FreeRTOS-thread-aware-debugging-on-static-RTOS/m-p/1174826#M6281</link>
      <description>&lt;P&gt;When using the static allocation version of FreeRTOS the task list in the debugging view does not populate.&amp;nbsp; Furthermore when configuring the the TAD machinery in freertos_tasks_c_additions.h there is not an option to select static when configuring the memory model.&lt;/P&gt;&lt;P&gt;The thread list does show the threads but nothing in the task list view&lt;/P&gt;&lt;P&gt;Is this not supported in the static mode of FreeRTOS?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Oct 2020 22:41:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/FreeRTOS-thread-aware-debugging-on-static-RTOS/m-p/1174826#M6281</guid>
      <dc:creator>alannilsson</dc:creator>
      <dc:date>2020-10-28T22:41:43Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS thread aware debugging on static RTOS</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/FreeRTOS-thread-aware-debugging-on-static-RTOS/m-p/1175429#M6287</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/68876"&gt;@alannilsson&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;You don't say which device you're working with, but I have TAD working with FreeRTOS on Kinetis devices.&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;The directions I used are from&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2018/08/02/tutorial-using-runtime-statistics-with-amazon-freertos-v10/" target="_self"&gt;Tutorial: Using Runtime Statistics with Amazon FreeRTOS V10&lt;/A&gt;&amp;nbsp;by&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/17173"&gt;@ErichStyger&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Let me know how this works for you,&lt;/P&gt;&lt;P&gt;myke&lt;/P&gt;</description>
      <pubDate>Thu, 29 Oct 2020 16:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/FreeRTOS-thread-aware-debugging-on-static-RTOS/m-p/1175429#M6287</guid>
      <dc:creator>myke_predko</dc:creator>
      <dc:date>2020-10-29T16:25:48Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS thread aware debugging on static RTOS</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/FreeRTOS-thread-aware-debugging-on-static-RTOS/m-p/1175465#M6288</link>
      <description>&lt;P&gt;The 'All-Stop' setting when setting up the launch config does not stick. &amp;nbsp;Delete all launch configs, create a new one and select 'All-Stop' -&amp;gt; does not work. &amp;nbsp;Stop debugging and open launch config properties and 'non-stop' is check marked. &amp;nbsp;Uncheck that and debug then it works.&lt;/P&gt;&lt;P&gt;This happens on both versions 10.2 &amp;amp; 11.1&lt;/P&gt;&lt;P&gt;In the end it is now working for me, case closed.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Oct 2020 18:34:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/FreeRTOS-thread-aware-debugging-on-static-RTOS/m-p/1175465#M6288</guid>
      <dc:creator>alannilsson</dc:creator>
      <dc:date>2020-10-29T18:34:03Z</dc:date>
    </item>
  </channel>
</rss>