<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックSWO Not working under Linux (Ubuntu)</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/SWO-Not-working-under-Linux-Ubuntu/m-p/1151753#M6123</link>
    <description>&lt;P&gt;Product: MCUXpresso IDE&lt;BR /&gt;Version: MCUXpresso IDE v11.2.0 [Build 4120] [2020-07-09]&lt;BR /&gt;Operating system: Linux&lt;BR /&gt;VM: Java HotSpot(TM) 64-Bit Server VM (64 bit)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Everything is working fine in the debugger except for the SWO functions (SWO profile, ...).&lt;/P&gt;&lt;P&gt;The same exact config and code has been tested on a Windows 10 computer and the SWO Profile works perfectly well.&lt;/P&gt;&lt;P&gt;What could be wrong on Linux so that this particular functionality of the debugger doesn't work?&lt;/P&gt;&lt;P&gt;Is there anything to try and install?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Thu, 10 Sep 2020 21:09:31 GMT</pubDate>
    <dc:creator>alexandrekral</dc:creator>
    <dc:date>2020-09-10T21:09:31Z</dc:date>
    <item>
      <title>SWO Not working under Linux (Ubuntu)</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/SWO-Not-working-under-Linux-Ubuntu/m-p/1151753#M6123</link>
      <description>&lt;P&gt;Product: MCUXpresso IDE&lt;BR /&gt;Version: MCUXpresso IDE v11.2.0 [Build 4120] [2020-07-09]&lt;BR /&gt;Operating system: Linux&lt;BR /&gt;VM: Java HotSpot(TM) 64-Bit Server VM (64 bit)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Everything is working fine in the debugger except for the SWO functions (SWO profile, ...).&lt;/P&gt;&lt;P&gt;The same exact config and code has been tested on a Windows 10 computer and the SWO Profile works perfectly well.&lt;/P&gt;&lt;P&gt;What could be wrong on Linux so that this particular functionality of the debugger doesn't work?&lt;/P&gt;&lt;P&gt;Is there anything to try and install?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Sep 2020 21:09:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/SWO-Not-working-under-Linux-Ubuntu/m-p/1151753#M6123</guid>
      <dc:creator>alexandrekral</dc:creator>
      <dc:date>2020-09-10T21:09:31Z</dc:date>
    </item>
    <item>
      <title>Re: SWO Not working under Linux (Ubuntu)</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/SWO-Not-working-under-Linux-Ubuntu/m-p/1162623#M6180</link>
      <description>&lt;P&gt;Hi Alexandrekral:&lt;/P&gt;&lt;P&gt;The SWO functionality depends on the target device. which device you are using?&lt;/P&gt;&lt;P&gt;The SWO also depends on the probe connection too. Only the most recent P&amp;amp;E debug probes do support SWO.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Sun, 04 Oct 2020 12:24:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/SWO-Not-working-under-Linux-Ubuntu/m-p/1162623#M6180</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2020-10-04T12:24:43Z</dc:date>
    </item>
  </channel>
</rss>