<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K64 UART1 first char is zero in MCUXpresso IDE</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/K64-UART1-first-char-is-zero/m-p/1065847#M5752</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One thing i can answer:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if the first command after reset is TX from k64 to host , I get extra zero&lt;/P&gt;&lt;P&gt;if the first command is host -&amp;gt; k64 and then k64-&amp;gt;host , there is no extra first zero.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so i think there is a bug in this scenario.&lt;/P&gt;&lt;P&gt;can some one confirm?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also , left the&amp;nbsp;invert problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 24 May 2020 18:41:18 GMT</pubDate>
    <dc:creator>eliarad2</dc:creator>
    <dc:date>2020-05-24T18:41:18Z</dc:date>
    <item>
      <title>K64 UART1 first char is zero</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/K64-UART1-first-char-is-zero/m-p/1065846#M5751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I setup a K64 uart1 to windows host ( c#)&amp;nbsp;&lt;/P&gt;&lt;P&gt;two thing i see&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. The first byte that being sent is always zero.&lt;/P&gt;&lt;P&gt;i am using the polling example ( modified to UART1)&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. the tx output fifo is inverted by default , so i needed to set the C3 tx fifo bit&amp;nbsp;&lt;/P&gt;&lt;P&gt;C3 = C3 | 0x10;&lt;BR /&gt; UART_WriteC3(COMM_UART, C3);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2&amp;nbsp;questions:&lt;/P&gt;&lt;P&gt;1. how to fix the first zero byte&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. why the default is that data are inverted?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Notes:&lt;/P&gt;&lt;P&gt;the RX is also inverted , so i changed RXINV in S2 to 1.&lt;/P&gt;&lt;P&gt;The RX( host to k64) does not have additional zero only the k64-&amp;gt;host have additional one zero after reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 May 2020 09:24:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/K64-UART1-first-char-is-zero/m-p/1065846#M5751</guid>
      <dc:creator>eliarad2</dc:creator>
      <dc:date>2020-05-23T09:24:35Z</dc:date>
    </item>
    <item>
      <title>Re: K64 UART1 first char is zero</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/K64-UART1-first-char-is-zero/m-p/1065847#M5752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One thing i can answer:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if the first command after reset is TX from k64 to host , I get extra zero&lt;/P&gt;&lt;P&gt;if the first command is host -&amp;gt; k64 and then k64-&amp;gt;host , there is no extra first zero.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so i think there is a bug in this scenario.&lt;/P&gt;&lt;P&gt;can some one confirm?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also , left the&amp;nbsp;invert problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 May 2020 18:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/K64-UART1-first-char-is-zero/m-p/1065847#M5752</guid>
      <dc:creator>eliarad2</dc:creator>
      <dc:date>2020-05-24T18:41:18Z</dc:date>
    </item>
    <item>
      <title>Re: K64 UART1 first char is zero</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/K64-UART1-first-char-is-zero/m-p/1065848#M5753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eli:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please attach your scope shot ? Rx line and Tx line？&lt;/P&gt;&lt;P&gt;Do you use the NXP TWR-board or Freedom Board? what else did you change, other than the UART1?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 07:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/K64-UART1-first-char-is-zero/m-p/1065848#M5753</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2020-05-26T07:50:57Z</dc:date>
    </item>
    <item>
      <title>Re: K64 UART1 first char is zero</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/K64-UART1-first-char-is-zero/m-p/1065849#M5754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel&lt;/P&gt;&lt;P&gt;I dont have scope shot.&lt;/P&gt;&lt;P&gt;just code.&lt;/P&gt;&lt;P&gt;I&amp;nbsp;am using FRDM k64&lt;/P&gt;&lt;P&gt;I&amp;nbsp;wrote the code on K64 and on host c# , and got the findings i described&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 15:22:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/K64-UART1-first-char-is-zero/m-p/1065849#M5754</guid>
      <dc:creator>eliarad2</dc:creator>
      <dc:date>2020-05-27T15:22:07Z</dc:date>
    </item>
    <item>
      <title>Re: K64 UART1 first char is zero</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/K64-UART1-first-char-is-zero/m-p/1065850#M5755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eli&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest you run the NXP released polling demo.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;boards\frdmk64f\driver_examples\uart\polling&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;Please also check the hardware connection to PC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;K64&amp;nbsp; uart tx&amp;nbsp; &amp;lt;--&amp;gt;&amp;nbsp; PC Rx&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;K64&amp;nbsp; uart rx&amp;nbsp; &amp;lt;--&amp;gt; PC tx&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regard&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2020 07:12:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/K64-UART1-first-char-is-zero/m-p/1065850#M5755</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2020-05-29T07:12:00Z</dc:date>
    </item>
  </channel>
</rss>