<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso IDEのトピックRe: MCUXpresso IDE 11.1.0 Breakpoint error message</title>
    <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-1-0-Breakpoint-error-message/m-p/1052839#M5673</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The customer was copy a project from one PC to another.&lt;/P&gt;&lt;P&gt;Perhaps the project was not export and imported properly so the files's directory was not align properly, right?&lt;/P&gt;&lt;P&gt;Can you reference a blog of the reported issue?&lt;/P&gt;&lt;P&gt;where in the project setting is this directory path that you have to change?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jun 2020 01:04:29 GMT</pubDate>
    <dc:creator>HeMyFAE</dc:creator>
    <dc:date>2020-06-17T01:04:29Z</dc:date>
    <item>
      <title>MCUXpresso IDE 11.1.0 Breakpoint error message</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-1-0-Breakpoint-error-message/m-p/1052837#M5671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;Dear TEch support,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While debuging a problem&amp;nbsp; I tried to set a breakpoint and got the following error message below:&lt;/P&gt;&lt;P&gt;"Breakpoint installation&amp;nbsp; failed : Unmatched quote" .&lt;/P&gt;&lt;P&gt;It prevents me from setting a breakpoint.&lt;/P&gt;&lt;P&gt;What does that means?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;hy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/113003i032A46318F881083/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2020 21:08:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-1-0-Breakpoint-error-message/m-p/1052837#M5671</guid>
      <dc:creator>HeMyFAE</dc:creator>
      <dc:date>2020-06-16T21:08:43Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE 11.1.0 Breakpoint error message</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-1-0-Breakpoint-error-message/m-p/1052838#M5672</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The last time this was reported it was because there was a strange character in the full directory path of the file. Breakpoints are set using the full path, so check the name. If there is a problem in the name, you’ll need to change it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2020 21:42:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-1-0-Breakpoint-error-message/m-p/1052838#M5672</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-06-16T21:42:13Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE 11.1.0 Breakpoint error message</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-1-0-Breakpoint-error-message/m-p/1052839#M5673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The customer was copy a project from one PC to another.&lt;/P&gt;&lt;P&gt;Perhaps the project was not export and imported properly so the files's directory was not align properly, right?&lt;/P&gt;&lt;P&gt;Can you reference a blog of the reported issue?&lt;/P&gt;&lt;P&gt;where in the project setting is this directory path that you have to change?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 01:04:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-1-0-Breakpoint-error-message/m-p/1052839#M5673</guid>
      <dc:creator>HeMyFAE</dc:creator>
      <dc:date>2020-06-17T01:04:29Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso IDE 11.1.0 Breakpoint error message</title>
      <link>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-1-0-Breakpoint-error-message/m-p/1052840#M5674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I refer to the location, on the disk, of the file. This is probably also the location of the workspace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the question I was referring to was thiis&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/532550"&gt;https://community.nxp.com/thread/532550&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if the project was Exported and Importes, there should be no problem. However if the directory name contains strange characters then this can cause the problem you are reporting.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2020 07:01:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-IDE-11-1-0-Breakpoint-error-message/m-p/1052840#M5674</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-06-17T07:01:31Z</dc:date>
    </item>
  </channel>
</rss>